×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 42672, Entry date: 10/09/1998
(0)
Rate

S5 modules that can be implemented in the S7-400 system using the adapter

  • Entry
  • Associated product(s)

QUESTION:
Which S5 modules can I implement in the S7-400 system using the adapter?

ANSWER:
Using the adapter you can implement the following S5 modules in the S7-400:

IP 240 (counter, position detector and positioning module)
IP 242 B (counter module)
IP 244 (temperature control module)
IP 246 I/A (positioning module for servo drives)
IP 247 (positioning module for step motors)
WF 705 (position detector module)
WF 706 (positioning module)
WF 707 (cam controller)
WF 721 (positioning module)
WF 723 A/B/C (positioning module)
IP 252 MC (synchronizing module)
IP 32 MC (High-performance synchronizing and positioning module)
IP 32 M (module for customized modules)

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.
Support to the statistics
With this function the IDs found are listed according to number (format .txt).

Generate list
Copy URL
Display page in new design
mySupport Cockpit