×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 42674746, Entry date: 06/15/2015
(4)
Rate

PCDiagBridge

  • Entry
  • Associated product(s)
PCDiagBridge is a software tool that makes available to the SIMATIC applications WinCC and WinCC flexible the diagnostics data provided by the DiagBase diagnostics software as well as messages from SITOP UPSs, WinAC RTX and WinAC RTX F.

Description
The diagnostics software allows you to recognize any possible disturbances with SIMATIC IPCs at an early stage. Error messages to the operating personnel help to avoid or reduce system downtimes.

You can use PCDiagBridge to monitor the following hardware and software components:

  • SIMATIC IPC hardware (fan speed, CPU temperature, CMOS voltage and mass storage, for example)
  • SITOP UPS (operating mode, error message, switch-off)
  • Operating and monitoring of the WinAC RTX / WinAC RTX F (Run/Stop, error display, operating mode)

The PCDiagBridge user interface provides you with all the relevant PC diagnostics data at a glance. Prepared templates for WinCC and WinCC flexible permit easy integration of the diagnostics data into the SIMATIC visualization system.

PCDiagBridge is available for downloading free of charge.

Note
The PCDiagBridge software will no longer be developed and adapted to current IPCs. If you would like diagnostics data from current IPCs or one of the following functions, we recommend using the SIMATIC IPC DiagMonitor diagnostics software.

  • Monitor networked SIMATIC IPCs
  • Read out and send error messages via OPC server, e-mail or SMS
  • Worldwide monitoring of SIMATIC IPCs via web browser

More information about DiagMonitor is available in Entry ID: 109477200 and on the website: www.siemens.com/simatic-pc.

Hardware requirements
PCDiagBridge can run on the following SIMATIC IPCs:
 

Panel PCs Box PCs Rack PCs
SIMATIC IPC277D SIMATIC IPC227D
SIMATIC HMI IPC477C
SIMATIC HMI IPC477C PRO
Panel PC 477B
SIMATIC IPC427C
SIMATIC Microbox PC 427B
SIMATIC HMI IPC577C
Panel PC 577B
SIMATIC IPC547D
SIMATIC IPC547C
SIMATIC Rack PC 547B
SIMATIC HMI IPC677C
Panel PC 677B
SIMATIC IPC627C
SIMATIC Box PC 627B
SIMATIC IPC647C
Rack PC 647B
SIMATIC Box PC 827B SIMATIC IPC847C
Rack PC 847B
SIMATIC Rack PC IL 43

Other supported products

  • All versions of WinAC RTX / WinAC RTX F
  • All SITOP UPSs with USB interface

Software requirements
PCDiagBridge runs on the following operating systems:

  • Windows 2000 Professional
  • Windows XP Professional
  • Windows XP Embedded (SIMATIC IPC Configuration)
  • Windows XP Embedded Standard 2009 (SIMATIC IPC Configuration)
  • Windows Server 2003 Edition (32-bit)
  • Windows Server 2008 Edition (32-bit)
  • Windows Vista Ultimate (32-bit)
  • Microsoft Windows 7 (32-bit)
       
The following software must also be installed in order to use PCDiagBridge:
  • Microsoft Visual Basic 6.0 runtime files
  • Microsoft WinSock Control 6.0 MSWINSCK.OCX
  • Microsoft Rich Textbox Control 6.0 RICHTX32.OCX
  • SIMATIC IPC DiagBase version V1.1 and higher
    Remark: The SIMATIC IPC DiagBase user interfaces "Management Explorer" and "Alarm Manager" can be operated in parallel, but are not requirements for PCDiagBridge. You can disable the automatic start of the Management Explorer and the Alarm Manager when Windows starts.  SITOP UPS USB driver FTD2XX.SYS (only if SITOP UPS is available)

Download
 
 

Version Download Date
Version 1.04.0008  Registrierung notwendig  pcdiagbridgesetup_v1_4_0008.zip (624,3 KB)  2013-04-28
Version 1.04.0007  Registrierung notwendig  pcdiagbridgesetup_v1_4_0007.zip (634,3 KB)  2013-02-22
Version 1.04.0003  Registrierung notwendig  pcdiagbridgesetup_v1_4_0003.zip (637,2 KB)  2011-03-01
Version 1.04.0001

 Registrierung notwendig  pcdiagbridgesetup_v1_4_0001.zip (636,9 KB) 

2010-07-26
Version 1.03.0001

 Registrierung notwendig  pcdiagbridgesetup_v1_3_0001.zip (635,3 KB) 

2010-03-02
Version 1.01.0001

 Registrierung notwendig  pcdiagbridgesetup_v1_1_0001.zip (720,4 KB) 

2009-02-25
Table 01

Further Information and Sample Applications
An example of how to incorporate PCDiagBridge and SIMATIC IPC DiagBase in your WinCC and WinCC flexible projects is available in Entry IDs: 29855065 (WinCC) und 31492549 (WinCC flexible).

The SIMATIC PC DiagBase software is available for downloading free of charge in Entry ID: 29316343.

 

 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
http://www.siemens.com/industrialsecurity.