×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ, Entry ID: 42681, Entry date: 09/01/2006
(0)
Rate

How do I link an S7-400 with S5 expansion units?

  • Entry
  • Associated product(s)

 
Description:
You can connect the following S5 expansion units to an S7-400:

EG 183U, EG 185U, EG186U, ER 701-2, ER 701-3

The interface is established via the IM463-2, which is plugged into the S7-400 CPU. Insert an IM 314 into the S5 expansion unit. Even expansion units which are connected decentrally via an IM 463-2 can be expanded centrally again.

You can find detailed information in the manual "S7-400 Module Data", chapter 7 (S5 interface in the IM 463-2)" in Entry ID 1117740.

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
http://www.siemens.com/industrialsecurity.