×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 42724613, Entry date: 05/26/2010
(1)
Rate

Language pack SinuTrain 7.5 ED2

  • Entry
  • Associated product(s)

The language packs for SinuTrain V07.05 ED2 are available for downloading.



SinuTrain programming and training on the PC

Description

A requirement for the installation of language packs is that SinuTrain V07.05 has been installed on the PC. Download the corresponding language pack (zip format) from the server and unpack ist. Execution of the unpacked EXE file installs the corresponding language pack for SinuTrain.

The following language packs are available for downloading:

Czech
Lang_V0705_CZ.exe ( 38824 KB )

Finnish
Lang_V0705_FI.exe ( 11128 KB )

Hungarian
Lang_V0705_HU.exe ( 34222 KB )

Japanese
Lang_V0705_JA.exe ( 15409 KB )

Dutch
Lang_V0705_NL.exe ( 11104 KB )

Polish
Lang_V0705_PL.exe ( 41466 KB )

Russian
Lang_V0705_RU.exe ( 51412 KB )

Swedish
Lang_V0705_SW.exe ( 31426 KB )

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.