×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 42931547, Entry date: 07/26/2011
(1)
Rate

Documentation of Production Processes with WinCC flexible

  • Entry
  • Associated product(s)

Task:
During the every day production process various production processes are started and terminated via the HMI operator panel.

This includes:

  • general operator actions
  •  adjusting of production parameters
  • output of process values
  • output of process alarms

For a number of operator actions it is difficult in retrospect to assign individual operator actions and alarms to a certain process/batch.

Solution:
The application is used to assign previously described points specifically to one “batch” in form of a “batch report” and hence document the “single” process.

A “batch report” (batch log) is required in many areas within industrial production, especially in the pharmaceutical, food and beverage industry.

Overview display:

 

The attached documentation contains a detailed instruction on how to realize the task.
The "zip-file" contains all required files to recreate the application.

Downloads

Content of Downloads

Download

Documentation  42931547_WinCC_flexible_Batch_Report_DOKU_V10_e.pdf ( 825 KB )
Code 
The zip-file contains the following file.
  • WinCC flexible configuration (Project_Code)
42931547_WinCC_flexible_Batch_Report_CODE_V10.zip ( 2815 KB )
Code 
The zip-file contains the following files.
  • Excel templates (Template_BatchReport_Excel_V1.2)
  • Example files (Sample_Data_BatchReport)
42931547_Template_Batch_Report_V10.zip ( 204 KB )

Software requirements:
The following software versions were used for implementing the example application.

  • WinCC flexible 2008 SP1
  • Microsoft Excel 2003

History

Version

Modification

06/2010 First issue

Keywords:
Pharma, Audit, GMP, Life Science, Validation, FDA 21 CFR Part 11

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.