×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 43033319, Entry date: 05/28/2010
(1)
Rate

Configurating of Cascade Control

  • Entry
  • Associated product(s)
The project example shows the application of cascade control to a simulated process with one main and one auxiliary process variable.

Objective of the Application
A cascade control structure can be established if, beside the main process variable, more system variables are measured and fed back as auxiliary process variables, creating subordinate control loops. Thus there is a master (or main) control loop and a slave (or auxiliary) control loop.
Cascade control is one of the most common control system structures in process plants.

The objective of this application note is to show the issues in configuration of cascade control loops that are particularly relevant to achieve fast dynamics and correct behaviour in all operating modes of real world applications.

Main contents
The following issues are discussed in this application note:

  • Interaction between master and slave controller with respect to controller tuning
  • Interaction between master and slave controller with respect to operating mode changeovers
  • Simulation example

Validity
This entry was created with SIMATIC PCS 7 V7.1, the procedure is transferable to PCS 7 V7.0 SP1 and higher versions.

Downloads
  Documentation - Configurating of Cascade Control (774,7 KB) 

History
05/2010 First release


Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.