×
Siemens Industry Online Support
Siemens AG
Tipo di articolo: Esempio di applicazione ID articolo: 43192621, Data articolo: 02/07/2010
(0)
Valuta

Demonstration system: STEP 7 Basic Innovations - SIMATIC S7-1200 Webcasts on the topic of online functions

  • Articolo
  • Riguarda prodotto/i

 

Webcast:
STEP 7 Basic Innovations


Fig. 01: Monitoring table

Topic
STEP 7 Basic, including WinCC Basic, is a comprehensive engineering system for efficient programming and configuration of SIMATIC S7-1200 controllers and SIMATIC HMI Basic panels. It provides you with intuitive and fast editors for programming and commissioning extensive automation solutions. The Webcasts in this entry show you the new SIMATIC S7-1200 innovations using selected scenarios.

Content
The following Webcasts discuss the online functionalities of STEP 7 Basic in detail. For example, you learn how to test the running of your user program via modifying and monitoring of tags. You will also be shown how to specifically determine differences of your project data using an offline/online comparison, and how to react to it.

  • Offline/Online comparison:
    STEP 7 Basic contains a comparison editor which displays the differences of your offline and online project data. The Webcast shows you the contained functionalities, in particular how to specifically localize and repair differences in the program code.
  • Monitoring and modifying of tags:
    In STEP 7 Basic tags can be modified and monitored in the program code itself, as well as via the PLC tag table. The Webcast introduces both variants to you and also discusses the Forcing of tags function.

Operation
These audio Webcasts can be played without further software. Simply load the respective zip-file onto your computer, unzip the exe-file and start it via mouse-click. The Webcast starts immediately and is operated via the menu bar of the player.

Download

Webcast

Download

Offline/Online comparison
(ca 12.1 MB, 2 minutes runtime)
Online_Comparison_V21_en_fullscreen.zip ( 8916 KB )
Monitoring and modifying of tags
(ca 13.4 MB, 2 minutes runtime)
Online_Monitor_V21_en_fullscreen.zip ( 9788 KB )

History

Issue

Modifications

06/2010 First issue

Further Information 
Further Webcasts on the new STEP 7 Basic innovations are available in the following entries of the Applications & Tools Portal.

Title

Link

Demonstration system: STEP 7 Basic Innovations - SIMATIC S7-1200 Webcasts on the topic of Devices & Networks 43192620
Demonstration system: STEP 7 Basic Innovations - SIMATIC S7-1200 Webcasts on the topic of intelligent drag and drop and using PLC tags 43192840
Demonstration system: STEP 7 Basic Innovations - SIMATIC S7-1200 Webcasts on the topic of programming SIMATIC HMI Basic panels 43192951
Demonstration system: STEP 7 Basic Innovations - SIMATIC S7-1200 Webcasts on the topic of PLC programming 43192952
Demonstration system: STEP 7 Basic Innovations - SIMATIC S7-1200 Webcasts on the topic of portal and project views, as well as the Siemens information system 43192953
Further information on STEP 7 Basic is available on the Siemens product pages STEP 7 Basic for S7-1200

Avvertenze di sicurezza
Per proteggere l’infrastruttura tecnica, i sistemi, i macchinari e le reti da minacce cyber, è necessario implementare (e salvaguardare continuamente) un concetto IT Security complessivo che sia conforme agli standard della tecnica correnti. I prodotti e le soluzioni di Siemens formano solo una parte di tale concetto. Ulteriori informazioni sulla Cyber Security si trovano sotto
https://www.siemens.com/cybersecurity#Ouraspiration.