×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 4328169, Entry date: 01/08/1997
(0)
Rate

Customized Design for C7 Control Systems

  • Entry
  • Associated product(s)
                                                                            

                                                                            

Concerns products with the Catalog Nos.:                                    

                                                                            

6ES7623-1AE00-0AE3    SIMATIC C7-623,    control system                     

6ES7624-1AE00-0AE3    SIMATIC C7-624,    control system                     

6ES7626-1AG00-0AE3    SIMATIC C7-626,    control system                     

6ES7626-2AG00-0AE3    SIMATIC C7-626 DP, control system                     

                                                                            

The above C7 control systems can now be obtained in                         

customized design versions.                                                 

                                                                            

The following design changes are possible:                                  

- Own company logo                                                          

- Background color and keycap color                                         

- Color of the front casing                                                 

- Permanent inscriptions of the keys                                        

  (labelling strips can no longer be used then)                             

  The system keys (figures 0 to 9, ENTER, HELP etc.) retain                 

  their function, so that their inscriptions should preferably              

  not be altered to avoid problems when technical support is                

  needed and when carrying out standard HMI functions.                      

                                                                            

The following cannot be changed:                                            

- Position, quantity and functions of the keys                              

- Position and size of the display                                          

- Position, size and labelling of the C7 CPU LEDs                           

                                                                            

Standard RAL colors are used for the color design.                          

                                                                            

Your SIMATIC contact at your local Siemens office will gladly               

supply you with more information and prices.                                

                                                                            

                                                                            

                ---------------------------------                           





Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.