×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 4329704, Entry date: 04/11/1997
(0)
Rate

STEP 7-Micro/DOS and Manuals - New Versions

  • Entry
  • Associated product(s)
                                                                            

Concerns products with the Catalog Nos.:                                    

                                                                            

6ES7 810-2DA00-0YX0    STEP 7 Micro/DOS, single license                     

6ES7 810-2DA00-0YX1    STEP 7 Micro/DOS, copy license                       

6ES7 810-2DA00-0YX3    STEP 7 Micro/DOS, update                             

6ES7 901-3BF00-0XA0    PC/PPI cable for PG/PC on-line operation             

6ES7 810-2DA10-8AA0    STEP 7 Micro/DOS Manual, German                      

6ES7 810-2DA10-8BA0    STEP 7 Micro/DOS Manual, English                     

6ES7 810-2DA10-8CA0    STEP 7 Micro/DOS Manual, French                      

6ES7 810-2DA10-8DA0    STEP 7 Micro/DOS Manual, Spanish                     

6ES7 810-2DA10-8EA0    STEP 7 Micro/DOS Manual, Italian                     

                                                                            

                                                                            

STEP 7 Micro/DOS is now available with version 1.3. The new version         

offers the following new functions:                                         

                                                                            

- Support of the new S7-200 CPUs 210, 215 and 216.                          

- Support of the 13 new instructions of the CPUs 215/216.                   

- Access/editing of the complete variables memory in the CPUs 215/216.      

- Auto baud rate selection for PPI (9.6/19.2 kbaud).                        

- Expanded PLC-Utility No:10 (PLC Communications Parameters).               

- Import of a Micro/WIN OB1 file.                                           

                                                                            

A special feature of STEP 7 Micro/DOS is its low performance requirement    

on the hardware. It will execute from MS-DOS 5.0 or higher in a DOS window  

under Microsoft Windows 3.1, Windows for Workgroups 3.11 and Windows 95.    

A 286 microprocessor with 1 Mbyte main memory (of which at least 580        

Kbytes must be in the lower memory area) and 5 Mbytes of free hard disk     

space are sufficient as PG or PC hardware.                                  

                                                                            

The user manual has been reworked. The new version has to be ordered sepa-  

rately.                                                                     

                                                                            

                                                                            

_Compatibility:_                                                            

                                                                            

STEP 7-Micro/DOS V1.3 is fully compatible with all earlier Micro/DOS ver-   

sions. All programs that were generated with versions V1.0, V1.1, V1.2.1    

and V1.2.2 can be imported under STEP 7-Micro/DOS V1.3 and will execute.    

                                                                            

                                                                            

_Upgrading:_                                                                

                                                                            

The STEP 7-Micro/DOS update package (Catalog No. 6ES7 810-2DA00-0YX3) is    

available to upgrade all older Micro/DOS versions (V1.0, V1.1, V1.2.1,      

V1.2.2) to version 1.3. A prerequisite for the installation of the update   

is a version 1.0, 1.1, 1.2.1 or 1.2.2 on the hard disk.                     

                                                                            

                                                                            

                     ---------------------------------                      





Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.