×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 43433, Entry date: 03/06/1996
(0)
Rate

No on-line connection to AG 110A, AG 130A/K

  • Entry
  • Associated product(s)

PROBLEM:
STEP5 as from V1.0 doesn't come on-line with AG 110A, AG 130A, AG 130K

ANSWER:
The AG 110A, AG 130A and AG 130K controllers can only be processed on-line using a PG631 or PG670. The program structure of these AGs cannot be processed with STEP5 as from V1.0.

It is therefore not possible to connect up to these AGs with a PG635, PG675, PG685 and all PG7xx variants. This also applies for the EPROMs of these AG types. The contents of the EPROM cannot be read by STEP5.

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.