×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 43705887, Entry date: 10/11/2010
(1)
Rate

How are called and interconnected the SIMATIC Powerrate library blocks in STEP 7 and WinCC?

  • Entry
  • Associated product(s)

Description
This documentation shows how WinCC and STEP 7 with SIMATIC powerrate for WinCC blocks are used for an Energy Management solution. For this purpose, an example project has been created. The application is created using S7-300 and WinCC V7.0 SP1.

After installing SIMATIC powerrate for WinCC V3.0 SP1, you have to only copy the following Powerrate library blocks into the example project.


Fig. 01

The following illustration displays the most important components of the solution.


Fig. 02

The following illustration displays the program structure of the STEP7 Blocks.


Fig. 03

The attached documentation contains a detailed instruction, with "step by step configuration".
The "zip-file" contains the project.

Downloads
 

Content of Downloads

Download

Documentation  ( 3357 KB )
Code 
The zip-file contains the following file.
  • STEP7 and integrated WinCC project (without SIMATIC Powerrate library blocks( see above)).
( 52027 KB )
Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.