×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 43893636, Entry date: 12/20/2010
(0)
Rate

3NE 3NC 3NH 3NP 3KL 3KM - Load capacity of SITOR fuse links with NH-bases and NH-fuse switch disconnectors

  • Entry
  • Associated product(s)

QUESTION:

Which NH-bases or NH-fuse switch disconnectors can be used for semiconductor fuse links?
Howe high can SITOR fuse links in combination with NH-bases or NH-fuse switch disconnectors are be loaded?

 

ANSWER:

SITOR-fuse links can be used considering by maximum load capacity in our NH fuse switch disconnectors.

The maximum load capacity of SITOR fuse links with NH-bases and NH-fuse switch disconnectors are to be found in the catalog add-on ET B1 A0 (BETA Low-Voltage Circuit Protection Characteristic Curves for Catalog ET B1).

The actual version can be downloaded under:

http://www.automation.siemens.com/mcms/infocenter/content/en/Pages/order_form.aspx?nodeKey=key_9177913

 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?