×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 44016315, Entry date: 08/11/2010
(0)
Rate

STEP 7 Basic V10.5 Service Pack 2 Update 1

  • Entry
  • Associated product(s)

DESCRIPTION:

Update 1 enables automatic recognition of an integrated SD-card reader. In isolated cases the user previously had to insert the card reader manually via "Add User-defined Card Reader".

The update is also required to run the Field PG M3 with pre-loaded software 04/2010. Future pre-loaded software versions will include the update automatically.

Installation requirement: STEP 7 V10.5 SP2

Free download of update 1 for STEP 7 Basic V10.5 SP2:
Update 1 for STEP 7 Basic V10.5 SP2 ( 2117 KB )
This free download comprises the update 1 for STEP 7 V10.5 SP2 and can only be installed, if STEP 7 V10.5 SP2 is installed already.

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.