×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ, Entry ID: 44356678, Entry date: 07/18/2017
(2)
Rate

What is the power consumption or power dissipation of the SIMATIC HMI operator panels?

  • Entry
  • Associated product(s)
With SIMATIC HMI operator panels the power dissipation is only insignificantly less than the power consumption.
The values for power consumption are therefore almost identical to the maximum and minimum power dissipation.
Note that these values change when IO devices (a USB mouse, for example) are connected to the operator panel. Please refer to the relevant device manuals for the power consumption and the permissible range of the rated voltage.

Please respect the required minimum spacing when installing the devices. Please refer to the relevant device manuals for the power consumption and the permissible range of the rated voltage.

Please respect the required minimum spacing when installing the devices.

Additional Keywords
Current, Power consumption, Voltage

Security information
In order to protect plants, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art industrial security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about industrial security, please visit
http://www.siemens.com/industrialsecurity.
ProductSupport.EntityResultListTitle
ProductSupport.EntityResultListDescription

ProductSupport.EntityResultListButtonText
Copy URL
mySupport Cockpit
Related links