×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 44908868, Entry date: 09/03/2010
(2)
Rate

Signal Smoothing-in-Control-Loops

  • Entry
  • Associated product(s)
Objective of the application is the filter implementation and parameter setting as well as consequences of different filter time constants are shown, using the example project "APL_Example_EU".

Objective of the Application
Almost any real sensor device for the measuring of process values of control loops delivers signals, which are disturbed by typically high-frequency noise. Nevertheless the requirements for the control loop with respect to fast dynamics and moderate movements of the actuator are to be fulfilled as good as possible. Therefore signal noise is suppressed by a filter, and the proper choice of the filter time constants is a major issue.

Main contents
The following issues are discussed in this application note:

  • Interaction between the signal filtering and the controller
  • Simulation example

Validity
This entry was created with SIMATIC PCS 7 V7.1, the procedure is transferable to PCS 7 V7.0 SP1 and higher versions.

Downloads
  Documentation - Signal Smoothing-in-Control-Loops (868,5 KB) 

History
09/2010 First release

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?