×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 45336072, Entry date: 10/04/2010
(0)
Rate

SIMATIC WinCC V7.0 SP2 ASIA Released for Delivery

  • Entry
  • Associated product(s)

With immediate effect, SIMATIC WinCC V7.0 SP2 ASIA  has been released for delivery. SIMATIC WinCC V7.0 SP2 ASIA  is an independent and complete product and will replace the direct predecessor variant SIMATIC WinCC V7.0 SP1 ASIA. Sales of   SIMATIC WinCC V7.0 SP1 ASIA will end with the availability of SIMATIC WinCC V7.0 SP2 ASIA.

SIMATIC WinCC V7.0 SP2 ASIA is available as free download from the Internet for the previously delivered version WinCC V7.0 SP1 ASIA, from the download pages of the SIMATIC Customer Support (entry ID WinCC V7.0 SP2 ASIA: 44453021). There will be no automatic distribution of the service pack following a previous Hotfix shipment.

1. Delivery release

In addition to the Asian version SIMATIC WinCC V7.0 SP2 ASIA basic packages, the following WinCC options are also released, resp. are compatible:

  • WinCC/Server V7.0
  • WinCC/Redundancy V7.0
  • WinCC/User Archives V7.0
  • WinCC/Web Navigator V7.0
  • WinCC/DataMonitor V7.0 
  • WinCC/Connectivity Pack V7.0 
  • WinCC/Connectivity Station V7.0
  • WinCC/Central Archive Server V7.0 SP2 ASIA
  • WinCC/ODK V7.0

We will inform you separately about the delivery release resp. the compatibility test for the following WinCC basic packages / options:

  • WinCC/IndustrialX V7.0 SP1
  • WinCC/CalendarScheduler V7.0 SP2
  • SIMATIC Maintenance Station 2010
  • SIMATIC ProAgent V7.0 SP1
  • SIMATIC WinCC DowntimeMonitor V7.0 SP2
  • SIMATIC WinCC IndustrialDataBridge V7.0 SP2

Other versions of these options will not run with SIMATIC WinCC V7.0 SP2 ASIA, resp. have not been tested for compatibility.

2. Details

The scope of functions of SIMATIC WinCC V7.0 SP2 ASIA is the same as that of the standard variant SIMATIC WinCC V7.0 SP2. Technical details are described in the delivery release of SIMATIC WinCC V7.0 SP2 (see entry ID: 44451711).

3. Ordering data

Ordering Data WinCC V7.0 SP2 ASIA ( 41 KB )

 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.