×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 46179468, Entry date: 10/28/2010
(2)
Rate

SINAMICS G: Speed control of a ET200S FC/ET200pro FC using S7-300/400 (STEP 7 V5) with PROFINET

  • Entry
  • Associated product(s)

Task:

One or several ET200S FC frequency converters (FW 3.0 or higher) or ET200pro FC are being used in a plant or system. Communication that goes beyond the standard telegram 1 is to be established using these frequency converters.

With the launch of the ET200S FC (FW1.x), a partner block FB100 (V2.2) was also provided. This partner block can no longer be used for the currently available ET200S FC (FW 3.0).


Solution:
A new FB100 (V 3.0) was developed to resolve this problem; this runs from firmware version V3.0 and higher of the ET200S FC and ET200pro FC. During development, special emphasis was placed on keeping the differences to the previous FB100 (V2.2) to a minimum regarding its behavior and how it is controlled.


 Downloads

Content of downloads

Download

Documentation
ET200S_proFC_V30_EN.pdf
ET200S_proFC_V30_EN.pdf ( 585 KB )
project
ET200_FC_STARTUP.zip
ET200_FC_STARTUP.zip ( 773 KB )

Keywords: motioncontrol_apc_applications

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.