×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 47203110, Entry date: 01/25/2011
(0)
Rate

Service Pack 6 for SIMATIC iMap STEP 7 AddOn V3.0

  • Entry
  • Associated product(s)

Service Pack 6 (SP6) for SIMATIC iMap STEP 7 AddOn V3.0 has been released for delivery. It will be included on the DVD of STEP 7 V5.5, as well as on the STEP 7 Professional 2010 DVD. It is also available for free downloading via the Internet.

The SIMATIC iMap STEP 7 Add-On software package enables STEP 7 users to create PROFINET components without having to install SIMATIC iMap.

What’s NEW in Service Pack 6?

In SIMATIC iMap STEP 7 AddOn V3.0 SP6 provides the following new features:

New operating systems

The SIMATIC iMap STEP 7 AddOn V3.0 SP6 now supports the following additional operating systems:

  • MS Windows 7 Professional 32 Bit
  • MS Windows 7 Ultimate 32 Bit

New PROFINET devices

SIMATIC iMap V3.0 SP6 now supports the creation of PROFINET components from the following PROFINET IO controllers:

  • Devices with media redundancy
  • Shared IO Devices as Singleton components
  • WinAC: WinAC RTX (F) 2009 and higher
  • S7-modular Embedded Controller: EC31-RTX (WinLC RTX (F) EC)

More information on SIMATIC iMap STEP 7 AddOn V3.0 SP6 is available from the files:

How to obtain the Service Pack

The following options exist to obtain the Service Pack:

  • Download
    As usual, we are offering a free download.

  • Service Pack 6 for SIMATIC iMap STEP 7 AddOn V3.0 included on the installation CD of STEP 7 V5.5 and STEP 7 Professional 2010
    The SIMATIC iMap STEP 7 AddOn version V3.0 SP6 is included on the installation CD 2 of STEP 7 version V5.5 und STEP 7 Professional 2010. This means that all customers with a Software Update Service agreement for STEP 7 or STEP 7 Professional 2010 will get the SIMATIC iMap STEP 7 Add-On automatically.

 

Installation requirements for the Service Pack:
Installation of the SIMATIC  iMap STEP 7 Add-On necessitates STEP 7 including NCM for Industrial Ethernet and PROFIBUS. Please ensure that one of the following SIMATIC STEP 7 software packages is installed:

  • STEP 7 V5.4 and higher
  • STEP 7 Professional Edition 2006 and higher

It is not necessary that an older version of the SIMATIC iMap STEP 7 Add-On is installed. For the support of the new functionality in V3.0 SP6 you require STEP 7 V5.5 and higher.

Note:
If STEP 7 is not installed at all, or if an older version of STEP 7 than specified above is installed, the SIMATIC iMap STEP 7 Add-On cannot be installed.

Installation:

  • Please unpack the ZIP file to a temporary folder, and
  • Start the installation by calling "Setup.exe"

Service Pack 6 for SIMATIC iMap STEP 7 AddOn V3.0:
SIMATIC_iMap_STEP7AddOn_V30_SP6.zip ( 30775 KB )

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.