×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 47203711, Entry date: 12/23/2010
(0)
Rate

Service Pack 2 for SIMATIC iMap V3.0

  • Entry
  • Associated product(s)

Service Pack 2 (SP2) for SIMATIC iMap V3.0 has been released and can be downloaded free of charge from the Internet.

What’s NEW in Service Pack 2?

SIMATIC iMap V3.0 SP2 now supports the following additional MS Windows operating systems:

  • MS Windows 7 Professional 32 Bit
  • MS Windows 7 Ultimate 32 Bit
  • MS Windows 7 Enterprise 32 Bit
  • MS Windows XP SP3
  • MS Windows Server 2008

To be able to use the new functionalities you require SIMATIC iMap STEP 7 AddOn V3.0 SP6 (entry ID 47203110).

How to obtain the Service Pack

The following options exist:

  • Download
    As usual, we are offering a free download

Installation requirements for the Service Pack:

The Service Pack can be installed directly over the existing SIMATIC iMap V3.0 software.

Installation:

  • Start the installation by calling "SIMATICiMap3.0.2.0.zip"
  • Installation is then started with "setup.exe".

Service Pack 2 for SIMATIC iMap V3.0:
 SIMATIC_iMap_V30_SP2.zip ( 138781 KB )

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.