×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 47521119, Entry date: 12/22/2010
(0)
Rate

What should you watch out with regard to the Oracle data base for WinCC/B.Data?

  • Entry
  • Associated product(s)

Oracle® Database versions and licensing
In order to use B.Data, an Oracle® Database 11gR2 32 Bit Standard Edition One, Standard Edition or Enterprise Edition is required. This database may be used for B.Data only. The customer himself is responsible for the correct licensing, the number of named users+ licenses and the compliance of the license. A definition of the different Oracle Database Editions as well as the Oracle’s licensing model can be found on the homepage at:

http://www.oracle.com/us/products/database/index.html
http://www.oracle.com/corporate/license/agreements.html

Licensing example
For the basic system of B.Data, running on a PC with 1 CPU and with Oracle Database 11gR2 32 Bit Standard Edition One installed, the following license configuration is recommended:
 

Component Required named user+ licenses
WINCC/B.DATA V5.2, BASIC SYSTEM,100 or
WINCC/B.DATA V5.2, BASIC SYSTEM,500 or
WINCC/B.DATA V5.2, BASIC SYSTEM,1.000 or
WINCC/B.DATA V5.2, BASIC SYSTEM,30.000
5

For additional functionality, the amount of named user+ licenses would increase:
 

Component Additional required named user+ licenses
WINCC/B.DATA V5.2, ACQUISITION 1

Notice
In addition, each B.Data user (Full Client/Web Client) and each Data Mobile device needs a named user+ license.
From a technical point of view, it is recommended to use the Enterprise Edition of Oracle Database 11gR2 32 Bit to store more than 200 million measured values.

System requirements

  • You have to install the Oracle database software version 11gR2, 32 Bit.
  • You have to install only Oracle database software without any database.
    Also no Oracle database has to be installed on the computer.

Suchbegriffe
Energiemanagement, Energy Management, Energie-Management

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.