×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 47885440, Entry date: 02/03/2011
(0)
Rate

How do you configure an ISO-on-TCP connection for data exchange between S7-300 and/or S7-400 by way of Industrial Ethernet CPs?

  • Entry
  • Associated product(s)
You can use the open communication through ISO-on-TCP connections for data exchange by way of the Industrial Ethernet CPs of S7-300 and S7-400.

Below we describe how to configure an ISO-on-TCP connection for sending and receiving data by way of an Industrial Ethernet CP of S7-300 and S7-400.

ISOonTCP_Connection_en.pdf ( 2121 KB )

The functions below are called in the user program of the CPU for sending and receiving data by way of configured ISO-on-TCP connections.

  • FC5 "AG_SEND" and FC6 "AG_RECV" for the S7-300
  • FC50 "AG_LSEND" and FC60 "AG_LRECV" for the S7-400

The entries below contain sample programs and instructions for programming the above-mentioned functions in the user programs of S7-300 and S7-400: 17853532 and 18513371.

Note
More information on communication over the Industrial Ethernet with S7-300 and S7-400 is available in the entries below.
 

Entry ID Description
26171811  What properties, advantages and special features are offered by the protocols TCP, ISO-on-TCP, UDP and ISO Transport?
22385024 How do you configure a TCP connection for data exchange between S7-300 and/or S7-400 by way of Industrial Ethernet CPs?
47885893 How do you configure a UDP connection for data exchange between S7-300 and/or S7-400 by way of Industrial Ethernet CPs?
47885244 How do you configure an ISO transport connection for data exchange between S7-300 and/or S7-400 by way of Industrial Ethernet CPs?
29737976 How do you program the communication blocks FB63 "TSEND", FB64 "TRECV", FB65 "TCON" and FB66 "TDISCON" in order to use the ISO-on-TCP protocol for data exchange by way of the integrated PROFINET interface of a CPU or by way of the CP443-1 Advanced?
30564821 Functions (FC) and Function Blocks (FB) for SIMATIC NET S7 CPs Programming Manual

 


Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.