×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 48174373, Entry date: 08/05/2013
(0)
Rate

WinAC Shutdown

  • Entry
  • Associated product(s)
Description of the problem The WinAC expansion Shutdown offers a direct shutdown of the PC straight from the PLC program. Functionality ...

Description of the problem
The WinAC expansion Shutdown offers a direct shutdown of the PC straight from the PLC program.

Functionality
When you use Shutdown it is possible to shut down the PC where WinAC is in operation, from the PLC program with one function call.

Examples of use
The Shutdown-FB can be used in example in conjunction with an UPS (uninterruptible power supply): After a given time the PC/PC’s can be shut down in a controlled way to avoid data loss in case of exceeding the UPS capacity and following power failure.

WinAC WinAC Shutdown Overview

More information about this driver can be obtained from the provided PDF-documents.

Obtaining
If you are interested, please contact your local sales manager.

Contacts worldwide

Content of Downloads Download
Documentation 48174373_WinAC_Shutdown_Doku_v17_en.pdf ( 1480 KB )
Flyer 48174373_WinAC_Shutdown_Flyer_en.pdf ( 95 KB )

Additional Keyword
motioncontrol_apc_applications, WinAC, communication

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.