×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 48205977, Entry date: 03/07/2013
(0)
Rate

Which safety functions can you use with the interpolation on the fail-safe Technology CPU?

  • Entry
  • Associated product(s)

Description
The fail-safe Technology CPU 317TF-2 DP unites three CPU functions in one device:

  1. Standard SIMATIC PLC
  2. Fail-safe PLC (with Distributed Safety)
  3. Motion Control

As from version V4.2 of S7 Technology (and the associated CPU firmware) it is also possible to perform interpolated travel with the Technology CPU.
The special points about using interpolated travel with the
Technology CPU in conjunction with the integrated safety functions of
Safety Integrated are explained in the attached PDF file.

48205977_TF-CPU_Interpolation_with_Safety_e.pdf ( 729 KB )

Note
The safety functions explained in the attached PDF file apply analogously to synchronized axes. In the case of activated safety functions the synchronized axes must be controlled via master axis. The path object technology functions named in the attached PDF file could not be used in combination with synchronized axes.

Additional Keywords
synchronism, synchronized motion, gear synchronization, cam disc, cam synchronization, synchronized axes, coupled axes, leading axis, following axis, master, slave, coordinated axes

 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.