×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 48283510, Entry date: 12/13/2011
(1)
Rate

Communication Between S7-300 Stations by Using SINAUT ST7 Telecontrol via Dedicated Line and Ethernet

  • Entry
  • Associated product(s)

Problem 
Two parallel pumps that feed into a common pipeline shall be controlled and monitored from a control center.

Solution
This automation solution uses the SINAUT ST7 Telecontrol system. Based on SIMATIC S7, this telecontrol system enables

  • the fully automated monitoring of substations,
  • the event-controlled data transmission in all networks and
  • the remote programming and diagnosis of subordinate stations.

The example project includes one master station which communicates with two other stations, whereby station 2 is used as a node station. The master and station 2 are connected via Industrial Ethernet. The connection between station 3 and station 2 is realized with a dedicated line.
Each CPU of the two stations includes a simple controller for the relevant pump. The pump signals are simulated by the user program.

This application discusses the following main points:

  • telecontrol with SIMATIC
  • TIM communication modules
  • SINAUT Object
  • connection configuration
  • programming with TD7onCPU
  • programming with TD7onTIM

Downloads

Contents of the downloads

Download

Documentation
Communication Between S7-300 Stations by Using SINAUT ST7 Telecontrol via Dedicated Line and Ethernet
48283510_SINAUT_WAN_e.pdf ( 998 KB )
Code 
STEP 7/SINAUT ST7 Project
48283510_SINAUT_WAN_CODE.zip ( 1015 KB )

Additional Information
Additional examples on SINAUT via (E)GPRS.
 

Titele

Link

SINAUT ST7 Telecontrol configuration examples in Ethernet, secure Internet and (E)GPRS environment Beitrags-ID: 23810112

Security Notice
Caution
The functions and solutions described in this article confine themselves to the realization of the automation task predominantly. Please take into account furthermore that corresponding protective measures have to be taken up in the context of Industrial Security when connecting your equipment to other parts of the plant, the enterprise network or the Internet. Further information can be found under the Content-ID 50203404.

Last Changes
Order number of Modem MD2 has been changed (Table 2-1)

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.