×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 48351511, Entry date: 08/18/2014
(2)
Rate

SINAMICS G120/G120P/G120C: CAN Bus EDS files for Control Units

  • Entry
  • Associated product(s)
The EDS file for CAN is required to operate  SINAMICS as a node on a CAN bus and announce the device to the configuration tool.

The tools usually provide the relevant import functions.

CAN bus EDS files for SINAMICS G120/G120P Control Units and G120C Inverter
Designation MLFB Firmware Suitable EDS file
G120C CAN 6SL3210-1KE..-..C1 V4.5   Registrierung notwendig  sinamics_g120c_v4-5.zip (3,8 KB)
V4.6   Registrierung notwendig  sinamics_g120c_v4-6.zip (6,3 KB)
V4.7   Registrierung notwendig  sinamics_g120c_v4_7.zip (6,3 KB)
CU230P-2 CAN 6SL3243-0BB30-1CA3 V4.5   Registrierung notwendig  sinamics_g120_v4-5.zip (3,8 KB)
V4.6   Registrierung notwendig  sinamics_g120_v4-6.zip (6,6 KB) 
V4.7   Registrierung notwendig  sinamics_g120p_v4_7.zip (6,6 KB)
CU250S-2 CAN 6SL3246-0BA22-1CA0 V4.6   Registrierung notwendig  sinamics_g120s_vector.zip (6,3 KB)
V4.7   Registrierung notwendig  sinamics_g120s_vector_v4_7.zip (6,4 KB)

Please observe the following note if you have any problems when starting up SINAMICS together with a CAN master:

The default value of the CANopen object 1000 hex "Device Type" is missing in the device description files (EDS file). As a result, a controller may lead to a fault and the startup may fail when uploading the object and comparing it with the value in the EDS file.

As the EDS files are pure test files, the user can add the following line in the entry for the CANopen object 1000 hex using the text editor:

EDS file Line to be inserted (example see below)
SINAMICS_G120.eds
SINAMICS_G120C.eds
DefaultValue=0x02010192

Example:
Entry of the CANopen object 1000h in an EDS

[1000]
ParameterName=Device Type
ObjectType=0x7
DataType=0x0007
AccessType=ro
DefaultValue=0x00020192
PDOMapping=0

 

Note
You can find the EDS file for CAN for SINAMICS S110, S120 under the followed link: 48802094

 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.