×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 48418663, Entry date: 05/18/2018
(6)
Rate

PCS 7 Unit Template "Distillation Column" using the example of the Chemical Industry

  • Entry
  • Associated product(s)
The "Distillation Column" unit template is based on a standardized and structured design of the automation program through the use of predefined equipment and the control modules. The example is used both as a basis for projects and as an overall standardization template.

The standardization of automation engineering for processing plants, such as in the chemical industry, is a major challenge. Different process steps and procedures, different equipment and flexibility in the production make the task even more difficult. This includes the plant structure according to the ISA-106. This specifies the lower four levels, i.e. plant area, unit, equipment and device. A plant area always consists of units. The units contain standardized equipment modules.

The example contains all typical components of a distillation column, its control, the required logic and the visualization. The application program was created using the APL (Advanced Process Library), which also contains a model predictive multi-variable controller. The multi-variable controller is the core component of the control strategy; it takes on the control of head and bottom temperature in the distillation column. Further controls are subordinate to the multi-variable controller.

Its utilization offers the following advantages:

  • A reduction of the knowledge necessary to develop applications
  • A decrease in the configuration effort
  • More flexible setup and adaptation due to equipment modules
  • Standardized structures
 


A distillation column as part of a process plant

Main contents
The following main points are explained in this application:

  • Structure of process tag charts
  • Configuration of the PID controllers
  • Configuration of the MPC controller
  • Modifying a disturbance variable (feed volume / feed concentration) and compensation through the MPC controller
  • Structure and application of the simulation
  • Task-related overview screens with APG (PCS 7 V8.1 sample project)

Delimitation
The following exceptional cases are not covered by this application:

  • Multi-substance distillation, i.e. columns with additional lateral extractions
  • Columns with gaseous head products, which require a different structure for the pressure control
  • Vacuum columns with a special pressure control structure
  • Stripper, i.e. columns without reinforcement part
  • Columns with no representative temperature as controlled variable

Validity
SIMATIC PCS 7 PCS 7 V9.0, PCS 7 V8.1 SP1, PCS 7 V8.0 SP1 and V7.1 SP1

Documentation and Sample Project for PCS 7 V9.0
  Documentation (4,1 MB)

You can download the example project for PCS 7 V9.0 in the Extranet-section of this entry. This Extranet section is only visible if have concluded a Managed System Services contract. Refer to the following link for detailed information: Managed System Services.

Documentation and Sample Project for PCS 7 V8.1 SP1
  Documentation (2,4 MB)
 Registrierung notwendig  PCS 7 V8.1 SP1 sample project with APG (227,2 MB)

Documentation and Sample Projects for PCS 7 V8.0 SP1 and PCS 7 V7.1 SP1
  Documentation (7,2 MB)
 Registrierung notwendig  PCS 7 V8.0 SP1 sample project (132,2 MB)
 Registrierung notwendig  PCS 7 V7.1 SP1 sample project (72,4 MB) 

Further Information
Equipment Modules for PCS 7 using the example of the Chemical Industry
PCS 7 Unit Template "Polymerization Reactor" using the example of the Chemical Industry
PCS 7 Unit Template “Stirred Tank Reactor” using the example of the Chemical Industry
PCS 7 Unit Template “Fermenter” using the example of the Chemical Industry
PCS 7 Unit Template “Dryer” using the example of the Chemical Industry
Integration of Advanced Process Graphics in SIMATIC PCS 7
Simulation of a PCS 7 stirred tank reactor with SIMIT Simulation Framework
Service Contracts - SIMATIC PCS 7 Lifecycle Services
Managed System Services overview page 

Last change
New project for PCS 7 V9.0 with Integration of Smart Alarm Hiding

Additional Keywords
Distillation Columns,  Unit Templates, chemical plants, projecting examples, rectification column, destillation

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
http://www.siemens.com/industrialsecurity.