Entry type:
Product note
Entry ID:
4891504,
Entry date:
07/24/2000
Rate
840D Release for general availability MMC 100.2 SW 5.3 (05.03.12)
-
Entry
-
Associated product(s)
The improved MMC 100.2 system software and the programming package for software release 5.3 (version 05.03.12) for SINUMERIK 810D/DE/840D/DE have been released for general availability and are, effective immediately, available from the plant. The software is supplied on the MMC 100.2 hardware or on data medium. The "Operator units management" option has also been released (in conjunction with NCU system software 5.3 and toolbox 5.3). Components which have been released: ==================================== MMC 100.2 hardware with MMC 100.2 system software 6FC5210-0DA00-1AA1 05.03.12 MMC 100.2 WIN32 configuring package on floppy disks single license 6FC5253-5AX50-3AB0 05.03.12 update 6FC5253-5AX50-3AB3 05.03.12 MMC 100.2 system software on CD-ROM single license 6FC5253-5AX00-3AG0 05.03.12 ö update 6FC5253-5AX00-3AG3 05.03.12 ö +-Patch MMC 100.2 05.01.45 +-MPI Installshield installation for MPI on PC +-System software 4.4 En/Ge +- MMC 100(real mode) 04.04.13 + 04.04.22 +- MMC 100.2(protected mode) 04.04.13 + 04.04.22 +-Language extensions SW 4.4 Fr/It/Sp +- MMC 100 04.04.14 + 04.04.22 +- MMC 100.2 04.04.14 + 04.04.22 +-System software 5.1, 5 languages +- MMC 100.2 (protected mode) 05.01.41 +- MMC WIN32 05.01.41 +- commissioning instructions, Section IM1 (pdf) +-System software 5.2, 5 languages +- MMC 100.2 (protected mode) 05.02.07 +- MMC WIN32 05.02.07 ö including keyboard driver +- commissioning instructions, Section IM1 and BE1 (pdf) +-System software 5.3, 5 languages +- MMC 100.2 (protected mode) 05.03.12 +- MMC WIN32 05.03.12 ö including keyboard driver +- cycle support 05.03.08 +- commissioning instructions, Section IM1 (pdf) Operator unit management (option) 6FC5253-0AE03-0AA0 This option can be purchased for each MMC/PCU which is integrated in the "Active/passive crowding" mechanism. The option has no machine data; but instead, has an entry in the NETNAMES.INI file and is activated corresponding to the documentation for operator unit management. Notes: - Screen languages: The system floppy disks have English as foreground language and German as background language. The application floppy disks, from software release 5.1 onwards, include German, English, French, Italian and Spanish which can be toggled between for the foreground and/or background language. The language floppy disks, SW 4.4 are included in a separate directory. - MMC 100.2 hardware, Order No. ÄMLFBÜ 6FC5210-0DA00-1AA1 will be changed- over from SW 4.4(V04.04.22)to SW 5.3 (V05.03.12) and supplied ex-factory. - When ordering the "current software release" Order No. ÄMLFBÜ 6FC5253- 0AX00-0AB0, the CD-ROM, Order No. ÄMLFBÜ 6FC5253-5AX00-3AG0 will be supplied; for Order No. ÄMLFBÜ 6FC5253-0AX50-0AB0, the set of floppy disks 6FC5253-5AX50-3AB0. - The software update service will be supplied with the various updates. New functions / function improvements from SW 5.2 to SW 5.3 =========================================================== Basic system: ------------- - The MMC 100.2 has been prepared for the extended functionality M:N (up to 8:8). The "Operator unit management" option includes the necessary active/passive crowding mechanisms. - Expansions for "Supplement operator interface": Displays can now be selected from the PLC, which were generated with "Supplement operator interface". - In displays, which were generated with "Supplement operator interface", bitmaps can be linked-in without first having to be converted. * Bitmap decompressed on FEPROM (for WIN32 decompressed on the harddisk) * Bitmap compressed in CST.ARJ (for Wizard standard cycles displays) * Bitmap compressed in CUS.ARJ (for Wizard customer cycles displays) - Editor: A jump can be made to the start of the file to be edited with "CTRL+POS1" and to the end with "CTRL+END". Operator area, machine: ----------------------- - The master spindle is now automatically displayed - Override display: For G0, the rapid traverse override is displayed in the basic machine display, otherwise the feed override - Inch/mm softkey: This softkey is only displayed in the NC operating modes if MD $MN_CONVERT_SCALING_SYSTEM, is not equal to 0 Operator area, parameters: -------------------------- - Access protection on the softkey basis shift is now possible (this involves the "Basis zero offset" and "Set actual value" softkeys) - It is possible to toggle between the tool manager "Standard MMC 100.2" and "ShopMill" using the display MD MM_TM_KIND_OF_TOOLMANAGEMENT. - MMC 100.2 standard tool manager: The number of possible magazines has been increased from 4 to 30 - The cursor memory is now also effective in the R parameter dialog - Cutting parameters 24 and 25 are now also compatible with ShopMill Operator area, program: ----------------------- - GUDs and MACs can now be edited in conformance with MMC 103; however, it is not possible to merge actual GUD values - Expanded contour computer: The individual contour elements of a step chain can be displayed as text (as before) and new, as icon. This is selected via MD $MM_PROGRAM_SETTINGS bit 3. Operator area, diagnostics: --------------------------- - "Set time" is now in conformance with MMC 103, also cyclic synchronization with the PLC time - "Percentage utilization display" is now in conformance with MMC 103 Operator area, 3D simulation: ----------------------------- - The operator area name has been changed from "Graphics" to "3D-Sim." Limitations: ============ The HLA module can be operated with MMC 100.2 from SW 5.3 onwards. When commissioning the HLA/ANA drive, the limitations MMC-D_ERLde33526,.27,.28,.30,.31 and .33 must be observed. Please contact your local Siemens department. Compatibility: ============== MMC 100.2 SW 05.03.12 can be combined with the 840D NCU software 4.x and 5.x or the 810D software 2.x and 3.x. Upgrade instructions: ===================== The upgrade instructions for MMC 100.2 (installation instructions for MMCWIN32) are included on the CD-ROM as "siemensd.txt" file in German and as "siemense.txt" in English, in the directory "sw_5_3/mmc100_2/disk01 (or "sw_5_3/mmcwin32/disk01). In case you require more information, please contact your local Siemens department.
Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Also available in the following languages:
- German
Entry belongs to product tree folder(s):
- Automation Technology Automation Systems SINUMERIK CNC Automation System CNC controls SINUMERIK 840 SINUMERIK 840D
- Automation Technology Automation Systems SINUMERIK CNC Automation System Operator components
- Automation Technology Automation Systems SINUMERIK CNC Automation System HMI software for CNC controls
- Automation Technology Automation Systems SINUMERIK CNC Automation System Archive CNC controls SINUMERIK 840D
Rate entry
Requests and feedback
What do you want to do?
- You have a technical question / problem: Ask the Technical Support
- You want to discuss in our forum and exchange experiences with other users
- You want to create CAx data for one or more products
- You would like to send us feedback on this Entry
Support to the statistics
With this function the IDs found are listed according to number (format .txt).
Copy URL
mySupport Cockpit
Product information