×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 48924746, Entry date: 05/25/2011
(7)
Rate

SINAMICS S110: PROFINET GSDML file

  • Entry
  • Associated product(s)
DESCRIPTION: GSDML file for the PROFINET IO for SINAMICS S110. This is required to operate the SINAMICS as a node on the PROFINET and announce the unit to the engineering tool. ...

DESCRIPTION:
GSDML file for the PROFINET IO for SINAMICS S110.
This is required to operate the SINAMICS as a node on the PROFINET and announce the unit to the engineering tool.
By way of example, engineering tools are here the existing and current STEP7 versions.
The relevant import functions are provided by the tools.

PROFIBUS GSD file for SINAMICS S110 Control Unit: 42705323

SINAMICS S110 Control Unit
 DesignationProduct  FirmwareSuitable GSD File 
 CU305 PN6SL3040-0JA01-0AA0 V4.4

  PN_GSDML_V23_S110.zip (9,1 KB) 1)

  pn_gsdml_v225_s110.zip (9,0 KB) 2)

  gsdml-v22-siemens-sinamics_s110-20120330.zip (8,4 KB) 3)

1) MRPD is supported

2) This GSD support PROFIsafe and Shared Device. It is installable from STEP7 V5.5, also from STEP7 V11. 
3) This GSD support all FW Version up to V4.4, but not PROFIsafe. This version should be used up to STEP7 V5.4 SP5. For higher STEP7 versions use the named GSD under note 1)

 

 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.