×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 48955585, Entry date: 03/02/2017
(2)
Rate

SIMOTION Message Handling

  • Entry
  • Associated product(s)
The Message Handling application collects all messages from the various sources of the SIMOTION system. These messages (e.g. from drives, technology objects, user-defined, etc.) are provided as actual messages and as message archive in a chronological order to the user.



The SIMOTION application engineer can further process the collected messages by reacting on alarm categories (fast stop, stop at end of cycle, etc.) or forwarding them to a higher-level system or displaying them on an HMI. The messages can be filtered in the HMI by message source or message class (information, warning, fault).

The application Message Handling can be integrated into your SIMOTION SCOUT (STEP 7 V5.x) project easily with the ProjectGenerator SIMOTION easyProject. In addition to the automatic program import or program update, the LDPV1 library (acyclic data exchange) required for the operation and a preconfigured program for the global resource management (pGlobalBufferManager) is also integrated automatically in the project. The SIMOTION IT web page for the Message Handling can also be integrated and loaded automatically.

ProjectGenerator: 51339107

SIMOTION LDPV1 library: 109479553

Downloads

  SIMOTION

    SIMOTION SCOUT
        SIMOTION Manual 11/2016 (1,7 MB)
        ReleaseNotes Message Handling SIMOTION V1.3.2 (10,7 KB)

Additional Keywords
motioncontrol_apc_applications, Meldehandling, Alarmhandling, Antriebsfehler, TO-Fehler, error handling, alarm handling, drive errors, TO-errors

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.