×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 49368600, Entry date: 03/24/2014
(0)
Rate

Remote Control of Operator Panel in Applications requiring Validation in the Pharmaceutical Environment

  • Entry
  • Associated product(s)
Task   In plants requiring validation it is important that all operator actions are recorded and that they can be assigned to the corresponding operators. In addition, there is the demand for “location-independent access to process data”. ...

Task  
In plants requiring validation it is important that all operator actions are recorded and that they can be assigned to the corresponding operators. In addition, there is the demand for “location-independent access to process data”.

A plant is to be operated with an operator panel. All relevant operator actions have to be recorded. In addition, it shall be possible to remote control the operator panel from a second operator panel.

Solution  

WinCC flexible/Sm@rtAccess
The WinCC flexible/Sm@rtAccess option enables client or server accesses from one panel to another. This is how the devices are "remote controlled“.
The current process values can be accessed plant-wide and their archiving and analysis can be provided. With the Sm@rtAccess option you relieve your field busses and you use a flexible solution for location-independent access to your plant.

WinCC flexible/Audit
The WinCC flexible/Audit option enables the recording of all relevant operator actions of an operator panel.
Storing the production data in electronic form offers many advantages compared with paper documentation, such as the simple recording and archiving of data. However, at the same time it has to be ensured that the data is forgery-proof and can be read at any time.

If two options are combined, the requirements to an application requiring validation are not fulfilled since there is no interlock for “remote control/remote service”.

The application example shows you a way how you can use the two options together. In addition to the use of the two options, server and client are synchronized through the SIMATIC HMI HTTP protocol.
Via this additional “service canal” the basic connection establishment and the interlock for the “remote control” takes place.

Downloads

Contents of the downloads

Download

Documentation 
49368600_WinCC_flexible_Audit_SmartAccess_en.pdf ( 1599 KB )
Code 
Sample project - Server
49368600_Server.zip ( 4972 KB )
Code 
Sample project - Client
49368600_Client.zip ( 4569 KB )

Further information

Title

Link

Application of WinCC WebNavigator in plant requiring validation Entry ID: 49516052
print WinCC flexible/Audit Entry ID: 36969886
Getting Started for WinCC flexible options Entry ID: 18657078


To stay informed about product updates as they occur, sign up for a product-specific newsletter. For more information, visit
http://support.automation.siemens.com.

Last change
Small changes on the documentation.

Additional keywords
Pharma, Audit, GMP, Life Science, Validation, FDA 21 CFR Part 11, SmartServer, SmartAccess, SmartClient


Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit