×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 49516052, Entry date: 07/28/2011
(0)
Rate

Documenting Operations Using WinCC WebNavigator

  • Entry
  • Associated product(s)

Problem
In the pharmaceutical industry, the food and beverage sector or in other industries, documentation of operator actions in terms of tracking and tracing is becoming increasingly important. Electronic documentation of operator actions ensures that all relevant operator actions during the production process are stored and, where necessary, acknowledged by the operator by an electronic signature and a comment.
The task is to allow full tracking and tracing, indicating who operated what when where. At the same time, it must be ensured that the logged operator actions are tamper-proof and that they can be read at any time. Operator actions must be recorded irrespective of whether they are performed over the Internet or on site using a web client or terminal client.

Solution
Using examples, this application shows the use of the SIMATIC WinCC WebNavigator option in conjunction with SIMATIC Logon to document process interventions with user-defined operator messages. It differentiates between the VBS and C script languages that are available in SIMATIC WinCC. The application also explains the difference between logging operations on a standard operator station and operations that are performed using a SIMATIC WinCC WebNavigator Client.

Downloads

Content of Downloads

Download

Documentation  49516052_WebNavigator_RecordOperatorActions_en.pdf ( 1299 KB )
Code  49516052_WebNavigator_RecordOperatorActions_CODE.zip ( 5608 KB )

Software requirenement
This application was created with WinCC V7.0 SP2.

History

Version

Modification

07/2011 First edition

Keywords
Audit, remote control, terminal, GMP, Pharma, Life Science, Validation, FDA 21 CFR Part 11

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.