×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 49639088, Entry date: 04/21/2011
(3)
Rate

Delivery release SIMATIC STEP 7 Professional V11

  • Entry
  • Associated product(s)


Intuitive, efficient and future-proof - the new engineering software programming the S7 controller

The products are based on Totally Integrated Automation Portal, the integrated work environment for the engineering software of IA and DT. STEP 7 Professional V11 is the engineering system for all SIMATIC controller classes (S7-1200, S7-300, S7-400); it also supports the additional functions of the new firmware, 2.0, for the S7-1200 controller (49741884). STEP 7 Professional 2010 remains in the product catalog and will continue to be maintained and further developed.
SIMATIC STEP 7 Professional V11 will be shipped together with SIMATIC WinCC Professional V11 (49740133) beginning 4/21/2011.
SIMATIC STEP 7 Professional V11 is immediately available for delivery. STEP 7 Basic V11 will be delivered as the successor to STEP 7 Basic V10.5 beginning 05/17/2011.

Product information

Functionality

Highlights

  • Portal view for quick, task-oriented starts

  • Intuitive user interface with high user friendliness

  • Clear configuration of devices and network topologies

  • Integrated mass data operations for efficient configuration

  • Common data management and universal symbolism

  • Powerful programming editor for efficient engineering

  • Optimum interaction between the controller and HMI in a work environment

  • System diagnostics as an integral part

  • Comprehensive library design

  • Scalability through the S7-1200, S7-300 and S7-400 controller families and beyond

  • Built-in password protection for program components

Powerful programming editor for efficient engineering

STEP 7 V11 provides powerful programming editors for programming S7 controllers: Ladder Logic (LAD) and Function Block Diagram (FBD) are available for all controllers, structured text (SCL), instruction lists (STL) and sequencer programming (GRAPH) are additionally available for the S7-300 and S7-400 controller families. The user is provided optimal system support for all tasks with features such as Drag&Drop, project-wide cross-reference lists, IntelliSense, etc.. STEP 7 V11 thus enables the user to create his application with the highest efficiency. Even sophisticated technological features such as loop-control or position control can be easily implemented in engineering software.

Intuitive user interface with high user friendliness

Editors that have been adapted to configuration tasks and processes, and the latest Windows technologies form the basis for the intuitive operating concept of STEP 7 V11.

Embedding the various editors in a common working environment ensures that all the latest data is available to users and guarantees a clear overview of project data at all times. 

Clear configuration of devices and network topologies

The configuration and parameter assignment for the hardware and network is another key task when creating an application. STEP 7 V11 supports the user with photo-realistic rendering and configuration of hardware modules. In the network view, users can simply build links between the various automation devices. In a view of the various networks (Profinet, Profibus, AS interface, etc.). In the online status, the diagnostic information of the modules are clearly displayed, thus providing the user an optimal overview of his plant even during operation and the commissioning.

Portal view for quick, task-oriented starts

The introduction to the engineering is much easier through the portal view. Even a beginner can navigate quickly and accurately to each task.

Maintenance personnel can also quickly familiarize themselves in the online view directly in the portal view, without having to first load a project.

Intelligent Drag&Drop

Project data are often reused at different locations of a project and linked in various editors. Intelligent Drag&Drop automatically creates these links for users. This way, data can be "dragged" directly from the PLC into an HMI picture and connected there. It is also possible to Drag&Drop hardware addresses directly from the device view into the programming editors. Connections between the elements are created automatically by the system in the background.

Comprehensive library design

The system features a comprehensive library design that enables reuse and easy standardization of frequently-used program parts.

Elements such as blocks, tags, alarms, HMI pictures, picture objects, individual modules or complete stations, including their parameters can be stored in local or global libraries. This makes them available for other programming tasks.

Investment security

With STEP 7 Professional V11, projects from STEP 7 V5.5 / STEP 7 Professional 2010 can easily continued to be used by migrating the program code and hardware configuration.

Editions

SIMATIC STEP 7 Professional V11 is the easy-to-operate, comprehensive engineering system for the latest SIMATIC S7-1200, S7-300, S7-400 controllers, which offers outstanding usability. WinCC Basic for configuring Basic Panels is included in the product package.

SIMATIC STEP 7 Basic V11 is easy-to-operate engineering system for the small, modular SIMATIC S7-1200 and related peripherals. It includes SIMATIC WinCC Basic for configuring SIMATIC Basic Panels. The delivery release of STEP 7 Basic V11 will take place separately on 02/05/2011.
 

System requirements

STEP 7 Professional / Basic V11 has been approved for use with the following operating systems (32-bit):

  • Microsoft Windows XP Home SP3 (STEP 7 Basic only)
  • Microsoft Windows XP Professional SP3
  • Microsoft Windows 7 Home Premium (STEP 7 Basic only)
  • Microsoft Windows 7 Professional
  • Microsoft Windows 7 Enterprise
  • Microsoft Windows 7 Ultimate
     
  • Microsoft Windows 2003 Server R2 Standard Edition SP2 (STEP 7 Professional only)
  • Microsoft Windows Server 2008 Standard Edition SP2 (STEP 7 Professional only)
     

 

Processor (min.)

RAM (min.)

Graphics (min.)

Recommended PC/PG hardware Core Duo, 2 GHz
or equivalent
2 GB 1280x1024

Compatibility with other SIMATIC products

STEP 7 Professional / Basic V11 (including WinCC Basic V11) may be installed on a computer side-by-side with other versions of STEP 7 (V5.4 / V5.5),  STEP 7 Basic V10.5, WinCC flexible (as of 2008) and WinCC (as of V7.0 SP2).

Software Update Service (SUS)

Customers who have an existing Software Update Service agreement for STEP 7 Professional can obtain an Upgrade as part of their contract. They may contact their local Siemens sales representative in order to get the Upgrade.
An automatic delivery of all STEP 7 Professional SUS customers will be provided with Service Pack 1 of STEP 7 Professional V11.
Customers who have an existing Software Update Service agreement for STEP 7 Basic will obtain an Upgrade of STEP 7 Basic V11 automatically as part of their contract.
A conversion package for STEP 7 Professional SUS is provided to STEP 7 Software Update Service customers.
 

Updating software for Field PG M3

An upgrade to V11 is initially provided for all Field PG M3 orders (except trial version) made after the delivery release of STEP 7 Professional V11. A customized Field PG M3 installation will be available in May 2011.
A separate sales/delivery release will be made for the new Field PG M3 software.

Ordering information

Name

Order number

STEP 7 Basic V11, Trial License 6ES7822-0AA01-0YA7

STEP 7 Basic V11, Single License

6ES7822-0AA01-0YA0
STEP 7 Professional V11,Trial License 6ES7822-1AA01-0YA7

STEP 7 Professional V11, Floating License

6ES7822-1AA01-0YA5
Upgrade STEP 7 Prof 2006/2010 auf STEP 7 Prof. V11, Floating License 6ES7822-1AA01-0XE5
PowerPack & Upgrade STEP 7 V5.4 to STEP 7 Prof. V11, Floating License 6ES7822-1AA01-0XC5
PowerPack STEP 7 Basic V11 to STEP 7 Prof. V11, Floating License 6ES7822-1AA01-0YC5
Upgrade STEP 7 Basic V10.5 to STEP 7 Basic V11, Single License 6ES7822-0AA01-0YE0
SUS STEP 7 Basic 6ES7822-0AA00-0YL0
SUS STEP 7 Basic compact* 6ES7822-0AA00-0YM0
SUS STEP 7 Professional (TIA Portal) 6ES7822-1AA00-0YL5
SUS STEP 7 Professional compact (TIA Portal)* 6ES7822-1AA00-0YM5
SUS STEP 7 Professional (TIA Portal & Classic) 6ES7810-5CC04-0YE2
SUS STEP 7 Professional compact (TIA Portal & Classic)* 6ES7810-5CC00-0YM2

*SUS compact means that, regardless of the quantity ordered, only one data medium (a USB stick) containing the appropriate number of license keys and the corresponding number of CoLs is delivered.

Readme file

You can find for additional information on STEP 7 Professional in the accompanying readme file. You can view it in portable document format (pdf.)

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
http://www.siemens.com/industrialsecurity.