×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 49970441, Entry date: 12/22/2015
(15)
Rate

SIMATIC/SIMOTION OMAC PackML V3 Machine and Unit States

  • Entry
  • Associated product(s)
This software library provides a user-friendly basis for the configuration and use of an OMAC-compliant mode and state manager for SIMATIC and SIMOTION.

State-of-the-art packaging machines and lines are extremely versatile, and must provide high throughput rates with the highest possible degree of flexibility. Reducing the total cost of ownership and investment security are also crucial issues. The key in achieving these objectives is the usage of standards for mode and state management and data interface in the machine.
Big end customers expect such a standardized handling for the machine user in the line which consists of machines from different vendors that have the same usability and diagnostics. In addition a standardized access to the machine data from upper level systems has to be guaranteed to be able to e.g. analyze product flow, acquire machine operating hours or calculate performance data.

The software (based on ISA-TR88.00.02-2008) is integrated in the machine application in STEP 7 V5.x by using the ProjectGenerator SIMOTION easyProject for SIMATIC or SIMOTION. The calls of the blocks are created and also the possible modes and states in the machine are parameterized. In addition a template structure is provided where the transition logic can be entered by the user.

ProjectGenerator: 51339107

Data interface: 86302104

OMAC: www.omac.org

Downloads
Note: The software located in this section is based on ISA-TR88.00.02-2015

  STEP 7 Professional / Basic V13 SP2 (TIA Portal)
  For the usage in newer STEP 7 versions see corresponding system manuals (Compatibility of projects/PLC
  programs)

    SIMATIC S7-1200/S7-1500
        Manual SIMATIC 06/2015 (1023,7 KB)
       Registrierung notwendig  LPMLV30 SIMATIC V3.0.1 (1,3 MB)
       Registrierung notwendig  LPMLV30 Example SIMATIC V3.0.1 (STEP 7 Professional only) (8,2 MB)

    SIMOTION SCOUT TIA
       Registrierung notwendig  LPMLV30 Example SIMOTION V3.0.1 (STEP 7 Professional only) (7,7 MB)

  SIMOTION

    SIMOTION SCOUT / SIMOTION SCOUT TIA
       Registrierung notwendig  LPMLV30 SIMOTION V3.0.1 (54,1 KB)
      Manual see SIMATIC S7-1200/S7-1500

Additional Keywords
motioncontrol_apc_applications

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit