×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ, Entry ID: 50029532, Entry date: 12/28/2015
(7)
Rate

Which devices and modules are supported by STEP 7 Professional and WinCC Professional in the TIA Portal?

  • Entry
  • Associated product(s)
To create new TIA Portal projects or to migrate projects from older versions you must first check that the available hardware components are supported by the current version of TIA Portal.

Description
There are two options for this:

  • Use the TIA Portal Readiness Check Tool, which informs you whether the hardware in projects is supported by the current version of TIA Portal. You can call the Readiness Check Tool via Entry ID 60162195.
  • Use the list provided in the present entry to see which hardware components are supported by which version of TIA Portal.

The list below shows which modules and which version of TIA Portal are compatible with STEP 7 and WinCC.

50029532_HWSupportList_DOC_TIAV13_en.xls (496.0 KB)

Note
Information about the compatibility of the separate software products with each other is available in the Compatibility Tool. This tool provides the function with which you can select compatible software products or check the compatibility of existing configurations. You can call the Compatibility Tool in this entry: 64847781.

Additional Keywords
Hardware update

Security information
In order to protect plants, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art industrial security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about industrial security, please visit
http://www.siemens.com/industrialsecurity.