Entry type: FAQ, Entry ID: 50052548, Entry date: 03/06/2013
(0)
Rate

Why can you not access an enabled folder in Windows XP SP3 on a panel?

  • Entry
  • Associated product(s)

Description
On a panel it is not possible to access an enabled folder from a computer with the Windows XP SP3 operating system installed.

Background
After the security update KB2267632 of 12/2010 for Windows CE 5.0 from Microsoft it is no longer possible to access the enabled folders if the difference between the system times of a panel with Windows CE 5.0 and a PC with Windows XP SP3 is longer than two days. The security update prevents access in this case.

Remedy
Make sure that the system times of the two systems lie within two days of each other.

Note
This concerns panels as from Windows CE 5.0 with Images as from 12/2010.

Error details
Detailed error description
Help us to improve Online Support.
The page requested cannot be displayed. Please contact the webmaster.
Contact to webmaster