×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 50085730, Entry date: 06/28/2011
(5)
Rate

Updates for STEP 7 V11 and WinCC V11

  • Entry
  • Associated product(s)

DESCRIPTION:

This update is applicable to the following products:

  • STEP 7 Basic/Professional V11.0 (w/o Service Pack)
  • WinCC Basic/Comfort/Advanced/Professional V11.0 (w/o Service Pack)

New features and changes in update 2 compared to earlier version:

  • STEP 7: Conflict in the case of parallel installation with STEP 7 V5.5 / WinAC has been corrected
  • STEP 7: S7-1200 program memory requirement has been optimized
  • WinCC: Optimization of the dimming in Comfort Panels - image update
  • Includes update 1

Update 1:

  • STEP 7: Significant improvements with code generation.
  • WinCC Engineering: Touch recognition of the Comfort Panels has been optimized.
  • Hardware configuration: Handling has been significantly improved, e.g. when uploading to the devices.

Installation instructions:

  • Please only install the current update 2, because it already includes update 1
  • The current update 2 must be installed after each installation of STEP 7 V11 or WinCC V11.

Free download

This free download comprises the update for STEP 7 Professional V11, WinCC Basic/Comfort/Advanced/Professional, and can only be installed, if one of these products is already installed.

Update 2 for STEP 7 V11 and WinCC V11 (06/2011):
TIAP_V11_0_UPD2.exe ( 307221 KB )

Update 1 (included in update 2) for STEP 7 V11 and WinCC V11 (05/2011):
TIAP_V11_0_UPD1.exe ( 194811 KB )

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.