×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 50085753, Entry date: 05/23/2011
(0)
Rate

When using the CPU317TF-2 DP, why is generation of the safety program interrupted with the message "Initialization of the safety program could not be completed."?

  • Entry
  • Associated product(s)

Description
If the PROFIsafe start addresses at the DP DRIVE are not unique station-wide, generation of the safety program or compilation of the hardware configuration of the CPU 317TF-2 DP is aborted with this error message:

  • Save and Compile (320:48) - Initialization of the safety program could not be completed.


    Fig. 01
     
  • Save and Compile (1230:3000) - The system data could not be recreated because the configuration is inconsistent.


    Fig. 02

Therefore, you should make sure that the start address of the PROFIsafe messages at the DP DRIVE are unique station-wide, which means that modules that are configured centrally or remotely must have different start addresses.

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.