×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 50204569, Entry date: 06/21/2021
(34)
Rate

What are the requirements for installing STEP 7 Professional / Basic V17?

  • Entry
  • Associated product(s)
The information and links below give you an overview of the general requirements for installing STEP 7 (TIA Portal).

1. Installation of STEP 7 Professional / Basic V17 in parallel to other versions of STEP 7

The requirements for installing STEP 7 Professional / Basic V17 are available in the Product Information and in the manual:


2. Parallel operation online of STEP 7 (TIA Portal) V17 with earlier versions of STEP 7

There is no release for the parallel operation online of STEP 7 V5.7 or earlier and STEP 7 V17 (TIA Portal).

The parallel installation of

  • WinCC V17 Advanced with versions of WinCC pre WinCC V7.3 is not permitted,
  • WinCC V17 with WinCC V7.3, WinCC V7.4 or WinCC V7.5 is not permitted for WinCC V17 Professional and WinCC V17 Runtime Professional.

Note
Consider for the installation the information in the Compatibility Tool for Automation and Drive Technology.


3. Opening projects from earlier versions of STEP 7 (TIA Portal)

In STEP 7 Professional / Basic V17 the STEP 7 Professional / Basic project is automatically upgraded to V17 when opened if you have created the project with TIA Portal V13 SP1 (or higher). Projects from earlier versions of TIA Portal first have to be stored and compiled in one of those versions. More information is available in Entry ID: 109476392.
 

4. Compatibility with projects from STEP 7 STEP 7 V5.4 SP5 and higher

Using the "Project > Migrate Project..." function in STEP 7 Professional / Basic V17 you can migrate Program codes and hardware configurations created with STEP 7 V5.4 SP5 and higher to STEP 7 Professional / Basic V17. The STEP 7 projects that contain a configuration with WinCC or WinCC flexible can also be migrated to STEP 7 Professional / Basic V17  with the included WinCC flexible parts. Included configurations created with WinCC V7.0+SP2 or lower are currently not migrated as well. The following components must be installed on your computer for this:

  • STEP 7 V5.4 SP5 and higher

  • WinCC V7.0+SP2 and higher or WinCC flexible 2008+SP2 and higher

More information is available in the manual of STEP 7 (TIA Portal) under Migrating STEP 7 projects.

Note
You cannot migrate WinCC V7.0+SP1 or lower.


5. Repair of STEP 7 (TIA Portal) V17 software

If the installation of STEP 7 Professional / Basic V17 is defective or has been damaged by an event, you have the option of repairing the software.

  1. Insert the STEP 7 Professional / Basic V17 CD in your computer's CD drive.

  2. If the Setup program does not start automatically, open the "Start.exe" file.

  3. Select the language in which you want the dialogs displayed.

  4. Select the "Repair" option field and click the "Next >" button.

  5. Follow the instructions on the screen.

Note
If installation of STEP 7 STEP 7 Professional / Basic aborts and you receive the message that you must uninstall an earlier version of WinCC Professional beforehand even though you have already done the uninstallation, this might be due to a Registry code. In the Registry Editor you open the path "HKEY_LOCAL_MACHINE\SOFTWARE\Wow6432Node\Siemens\Automation\_InstalledSW\TIAP1x\TIA_ES_V1x\PrivateProperties\INST_TYPE_LEVEL_INTERNAL" and remove the item "4_0_Professional". Do a restart and then you can install STEP 7 Professional / Basic V17.


6. Uninstallation of STEP 7 Professional / Basic V17

You can uninstall STEP 7 Professional / Basic V17 in two ways:

  • Uninstallation via the Control Panel (in Windows 10)
  • Uninstallation using the SIMATIC STEP 7 Professional / Basic V17 CD

The uninstallation instructions are in the TIA Portal Information System under Starting to uninstall


7. Further Information


Important

This entry contains information about editing the Registry. You should make a backup copy of the Registry before editing it. More information on making a backup copy, restoring and editing the registry is available in the Microsoft Knowledge Base in Entry ID 256986. Incorrect use of the Registry editor can cause serious problems that affect the complete system and require a reinstallation. You use the Registry editor at your own risk.

Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.