What are the requirements for installing TIA Portal V17 (STEP 7 Professional / Basic, WinCC Professional / Advanced)?
-
Entry
-
Associated product(s)
1. Installation of STEP 7 Professional / Basic V17 and installation in parallel to other versions of STEP 7
The requirements for installing STEP 7 Professional / Basic V17 are available in the Product Information:
2. Parallel online operation of STEP 7 (TIA Portal) V17 with earlier versions of STEP 7
There is no release for the parallel operation online of STEP 7 V5.7 or older and STEP 7 V17 (TIA Portal).
It is not permitted to install
- WinCC V17 Advanced in parallel to WinCC versions previous to WinCC V7.3.
- WinCC V17 with WinCC V7.3, WinCC V7.4 or WinCC V7.5 is not permitted for WinCC V17 Professional and WinCC V17 Runtime Professional.
Note
Before installing you should refer to the notes in Compatibility Tool for Automation and Drive Technology.
3. Parallel installation of WinCC (TIA Portal)
3.1 Parallel installation of WinCC (TIA Portal) with WinCC V6/V7 | ||
It is not permitted to install | ||
- WinCC V17 Advanced in parallel to WinCC versions previous to WinCC V7.3. | ||
- WinCC V17 Professional and WinCC V17 Runtime Professional in parallel to WinCC V6.x or WinCC V7.x. | ||
This also applies for earlier versions of WinCC Professional and WinCC Runtime Professional. | ||
3.2 Parallel installation of STEP 7 with WinCC Professional | ||
Only specific versions are compatible for a parallel installation of STEP 7 with WinCC Professional. Note | ||
3.3 Upgrade installation of WinCC Professional | ||
A WinCC SQL Server instance is installed when WinCC Professional or WinCC Runtime Professional is installed. |
4. Opening projects from earlier versions of STEP 7 (TIA Portal)
In STEP 7 Professional / Basic V17, the STEP 7 Professional / Basic project is automatically upgraded to V17 when you open the project if you have created the project in STEP 7 (TIA Portal) V13 SP1 (or higher). Projects from earlier versions of TIA Portal first have to be stored and compiled in one of those versions. More information is available in Entry ID: 109476392.
5. Compatibility with projects from STEP 7 V5.4 SP5 or higher
Using the "Project > Migrate Project..." function in STEP 7 Professional / Basic V17 you can migrate programs and hardware configurations you have created in STEP 7 V5.4 SP5 or higher directly into STEP 7 Professional / Basic V17. The STEP 7 projects that contain a configuration with WinCC or WinCC flexible can also be migrated to the STEP 7 Professional / Basic V17 with the included WinCC flexible parts. Included configurations created with WinCC V7.0+SP2 or lower are currently not migrated as well. In this case, the following components must be installed on your computer:
STEP 7 V5.4 SP5 or higher
WinCC V7.0+SP2 or WinCC flexible 2008+SP2 or higher
Further information is available in the TIA Portal Information System under Migration of STEP 7 Projects.
Note
You cannot migrate WinCC V7.0+SP1 or lower.
6. Repair of STEP 7 (TIA Portal) V17 software
If the installation of STEP 7 Professional / Basic V17 is defective or has been damaged by an event, you have the option of repairing the software.
Insert the STEP 7 Professional / Basic V17 CD in your computer’s CD drive.
If the Setup program does not start automatically, open the "Start.exe" file.
Select the language in which you want the dialogs displayed.
Select the "Repair" option field and click the "Next >" button.
Follow the instructions on the screen.
Note
If installation of STEP 7 Professional / Basic aborts and you receive the message that you must uninstall an earlier version of WinCC Professional beforehand even though you have already done the uninstallation, this might be due to a Registry code. In the Registry Editor you open the path "HKEY_LOCAL_MACHINE\SOFTWARE\Wow6432Node\Siemens\Automation\_InstalledSW\TIAP1x\TIA_ES_V1x\PrivateProperties\INST_TYPE_LEVEL_INTERNAL" and remove the item "4_0_Professional". Do a restart and then you can install STEP 7 Professional / Basic V17.
7. Uninstallation of STEP 7 Professional / Basic V17
You can uninstall STEP 7 Professional / Basic V17 in two ways:
- Uninstallation via the Control Panel (in MS Windows 10).
Uninstallation using the SIMATIC STEP 7 Professional / Basic V17 CD.
Instructions for uninstalling are available in the TIA Portal Information System under Start Uninstallation.
8. Further Information
- TIA Portal - An Overview of the Most Important Documents and Links - Controller
- Delivery release of WinCC V14 SP1
Important
This entry contains information about editing the Registry. You should always make a backup copy of the Registry before editing it. More information on making a backup copy, restoring and editing the registry is available in the Microsoft Knowledge Base in Entry ID 256986. Incorrect use of the Registry editor can cause serious problems that affect the complete system and require a reinstallation. You use the Registry editor at your own risk.
- German
- Italian
- Spanish
- Chinese
Entry belongs to product tree folder(s):
- Automation Technology Industry software Automation software TIA Portal PLC programming STEP 7 Professional (TIA Portal)
- Automation Technology Industry software Automation software TIA Portal PLC programming STEP 7 Basic (TIA Portal)
- Automation Technology Industry software Automation software TIA Portal Visualization SIMATIC WinCC (TIA Portal) SIMATIC WinCC (TIA Portal) Engineering
- Automation Technology Industry software Automation software TIA Portal Visualization SIMATIC WinCC (TIA Portal) SIMATIC WinCC (TIA Portal) Runtime
- Automation Technology Automation Systems Industrial Automation Systems SIMATIC Software for SIMATIC Controller STEP 7 (TIA Portal)
- Automation Technology Industry software Automation software TIA Portal Visualization SIMATIC WinCC (TIA Portal) SIMATIC WinCC (TIA Portal) Runtime WinCC Runtime Professional
- You have a technical question / problem: Ask the Technical Support
- You want to discuss in our forum and exchange experiences with other users
- You want to create CAx data for one or more products
- You would like to send us feedback on this Entry