×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 50274052, Entry date: 05/20/2011
(0)
Rate

How is the permissible usage or usage location defined for SIPLUS extreme?

  • Entry
  • Associated product(s)
6AG1 SIPLUS extreme: Permissible usage or usage location.

Description
Devices of the SIPLUS extreme family are generally released for the following usage and usage locations.

  • Usage in fixed locations (as per EN60721-3-3)
    The product is firmly mounted and is operated permanently at one specific place. It is not designed for usage in different places, but short times are taken into account for manipulation during mounting, maintenance and on-site repairs and during interruptions of operation.

  • Weather protected usage location (as per EN60721-3-3)
    A usage location that is protected against the direct influence of weather conditions. Completely weather-protected usage location (site closed on all sides). Direct influence of weather conditions is completely shut out.
Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.