×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 50274157, Entry date: 02/09/2012
(0)
Rate

With SIPLUS extreme, what is the meaning of "100% relative humidity (RH)" and "Bedewing permissible"?

  • Entry
  • Associated product(s)
6AG1 SIPLUS extreme: 100% relative humidity (RH) and bedewing are permissible

Description
Devices of the SIPLUS extreme family have a coating (conformal coating) which permits 100% RH and bedewing.

Note
As far as possible, avoid commissioning electronic devices in a "bedewed" state, because in a few exceptional cases this might lead to temporary error messages/behavior. Here you have to let the device acclimatize (dry) at room temperature if you change the location.

High temperatures combined with natural fluctuations in temperature (day/night), solar radiation during continuous operation or bedewing during storage and transport are permissible and do not lead to faulty behavior or damage.

Contact

Technical AssistanceDepartmentDF FA SE
Tel. no.+49 (0)911 895 5900
E-mailtechnical-assistance@siemens.com
Websitehttp://www.siemens.de/siplus-extreme


Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit