Entry type: FAQ, Entry ID: 50562572, Entry date: 08/03/2011
(0)
Rate

Where do you find sample programs and documentation on communication between S7-400 (PROFINET IO controller) and S7-300 (I slave) incorporating an IE-to-PB link gateway?

  • Entry
  • Associated product(s)

Description
This entry contains sample programs and documentation on communication between S7-400 (PROFINET IO controller) and S7-300 (I slave) incorporating an IE-to-PB link gateway.
A CP443-1 Advanced is used, which is configured as a PROFINET IO controller, in the S7-400. The S7-300 is connected as an I slave to the PROFINET IO controller via an IE-to-PB link.

The sample program consists of a STEP 7 project containing the configuration of the S7-400 as a PROFINET IO controller, as well as the configuration of the S7-300 as an I slave.

QS_IE-PB-LINK-Routing.zip ( 321 KB )

The document below contains

  • An overview of the sample program and plant configuration used to create the sample programs
  • Information about installing and commissioning the sample program
  • Information about how to use the sample programs
  • Other notes, tips and tricks, etc.

NET_communication_from_IE_to_PB_via_routing_en.pdf ( 397 KB )

More information
More information about communication between PC station and SIMATIC S7 via network components is available in the entries below.
 

Description Entry ID
S7-CPs for Industrial Ethernet Configuration and Commissioning Part A - General Application 30374198
Functions (FC) and Function Blocks (FB) for SIMATIC NET S7 CPs Programming Manual 30564821
CPU-CPU Communication with SIMATIC Controllers (Compendium) 20982954
Network Gateway IE/PB Link PN IO for Industrial Ethernet / Manual Part BL1 19299692
From PROFIBUS DP to PROFINET IO 19289930
SIMATIC PROFINET System Description 19292127