×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 50708061, Entry date: 03/05/2019
(9)
Rate

Integration of Comfort Panels, Operator Panels and S7-300 Package Units in SIMATIC PCS 7 with PCS 7 Industry Library

  • Entry
  • Associated product(s)
Apart from the components directly related to the engineering process, many production plants include further machines and aggregates which also need to be controlled. In many cases, these so-called ‘Package Units’ (PU) are complete subsystem models for specific production tasks. Some of these PUs are equipped with plant components which are not part of the standard PCS 7 system.

Automation task
There is often a requirement to integrate plant components in PCS 7 like SIMATIC S7-300 CPUs, Operator Panels with WinCC flexible or Comfort Panels with WinCC comfort (TIA).

In addition to operation from the control station, there is often a requirement for the control and visualization of PCS 7 plant components close by the machine. Moreover, the use of various types of operation and display schemes, as well as different types of alarm systems make the integration into the higher-level process control system more complicated.

Solution
This application example provides different standardized options for the integration of S7-300 CPUs, Operator Panels and Comfort Panels in a SIMATIC PCS 7 system. The solutions are based on PCS 7 Industry Library (IL).




Benefits of the solution with PCS 7 Industry Library

  • Enables integrated and harmonic solutions of a process control task and thus an optimal operation of the whole process by reducing risk of operation failures
  • Amount of user specific functions will be reduced, this saves costs over the complete life cycle
  • Synergy effects regarding training and know-how transfer

This topic includes the following application examples:

  • Integration of S7-300 package units in SIMATIC  PCS 7 with PCS 7 Industry Library
    • communication management in the S7-400 CPU with "S7Put" and "S7Get"
    • configuration of the S7-300 CPU with IL for S7
  • Integration of Operator Panels in SIMATIC  PCS 7 with PCS 7 Industry Library and WinCC flexible
    (machine-based operation and monitoring via the operating panel)
  • Integration of Comfort Panels in SIMATIC  PCS 7 with PCS 7 Industry Library and WinCC Comfort (TIA Portal)
    (machine-based operation and monitoring via the operating panel)

Validity

  • SIMATIC PCS 7 V9.0 with SIMATIC PCS 7 Industry Library V9.0 Update 1 (Comfort Panels, Operator Panels and S7-300)
  • SIMATIC PCS 7 V8.1 with SIMATIC PCS 7 Industry Library V8.1 (Comfort Panels)
  • SIMATIC PCS 7 V8.0 with SIMATIC PCS 7 Industry Library V8.0 (S7-300 and Operator Panels)

Documents

PCS 7 V9.0 SP1
The PCS 7 Industry Library V9.0 provides technological blocks for the control and monitoring of actuators and sensors which are also suitable for operation in S7-300 CPUs (IL for S7), as well as interface blocks, which interact with the PCS 7 APL, for the connection of operator panels (IL for PCS 7). The block libraries are accompanied by a WinCC Comfort V14 library ("IL for WinCC Comfort) (starting from Industry Library V9.0 Update 1)  with preconfigured block icons and faceplates for visualization on the Comfort Panel.
 Integration of Comfort Panels and Operator Panels in SIMATIC PCS 7 (3,5 MB)
 Integration of S7-300 Package Units in SIMATIC PCS 7(3,2 MB)

PCS 7 V8.1 (Comfort Panels)
The PCS 7 Industry Library V8.1 provides additional components for configuring Compfort Panels in TIA Portal.
The functionalities of the IL correspond regarding design and philosophy to the standards of the Advanced Process Library (APL) of SIMATIC PCS 7.
  Integration of Comfort Panels in SIMATIC PCS 7 (11,9 MB)

PCS 7 V8.0 (S7-300 and Operator Panels)
The PCS 7 Industry Library V8.0 provides technological blocks for the control and monitoring of actuators and sensors which are also suitable for operation in S7-300 CPUs (IL for S7), as well as interface blocks, which interact with the PCS 7 APL, for the connection of operator panels (IL for PCS 7). The block libraries are accompanied by a WinCC flexible library with preconfigured block icons and faceplates for visualization on the Operator Panel.
  Integration of Operator Panels in SIMATIC PCS 7 (4,0 MB)
  Integration of S7-300 Package Units in SIMATIC PCS 7 (2,3 MB)

Further Information
Sales and Delivery Release: SIMATIC PCS 7 Industry Library V9.0
Sales and Delivery Release for SIMATIC PCS 7 Industry Library V8.1
Sales and Delivery Release for SIMATIC PCS 7 Industry Library V8.0
Integration of third-party systems with SIMATIC PCS 7/OPEN OS

Last change
Documentation added for the integration of Comfort Panels, Operator Panels and S7-300 Package Units in SIMATIC PCS V9.0 SP1.

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit