Entry type: Application example Entry ID: 50897766, Entry date: 05/19/2016
(8)
Rate

Diagnostic block for AS-i master modules with visualization via HMI or web browser (Archive version 2016)

  • Entry
  • Associated product(s)
Block package for the diagnostics of AS-i master modules, including visualization on HMI panels or web browser

For use of the ET 200SP modules CM AS-i Master ST and F-CM AS-i Safety we provide a separate diagnosis package. 109479103

The presented diagnostic block for AS-i master modules supports the following and other AS-i masters from the SIMATIC product range:

  • DP/AS-i Link 20E
  • DP/AS-i LINK Advanced
  • IE/AS-i LINK PN IO
  • CP 343-2P, CP 343-2

Task 
AS-Interface slaves are connected with a SIMATIC controller via gateways or communication modules. An individual evaluation of the diagnostic data of the AS-i masters and slaves in the STEP 7 user program supports the plant operator searching the failure in case of service, so that the failure-free operation could be re-established fast.

The requirement in this application is to show how with the aid of a universal diagnostic block from a library all for S7-300/400 and S7-1500 actual available AS-i master systems can be common diagnosed and visualized.

Solution
To simplify the AS-i diagnostic for the user, the present library contains a number of blocks to be able to conveniently evaluate and visualize the diagnostic data:

  •  in the user program: The read AS-i diagnostic data is ready for individual further processing in a data block.
  • on HMI panels: The library includes blocks that serve as interface between HMI panel and CPU.
  • via web browser: SIMATIC CPUs with PROFINET interface provide the opportunity to access CPU variables with the help of individually designed web pages provided by the system. The library includes blocks that serve as interface between user-defined web pages and CPU. 

The diagnostic blocks were realized for the S7-300/400 and S7-1500 CPU.

WinCC flexible visualization
The diagnostics user interface is realized using the depending AS-Interface visualization block:


Image 01
 
Web visualization
The web user interface is realized using the depending AS-Interface visualization block and javascript:


Image 02

Downloads

  1. S7-1500 in TIA Portal V13 SP 1
     Registrierung notwendig  Project (TIA Portal V13 SP1) (18,1 MB)
      Documentation (1,5 MB)

  2. S7-300 in TIA Portal V13 SP 1
     Registrierung notwendig  Project (TIA Portal V13 SP1) (20,0 MB)
      Documentation (1,5 MB)

  3. S7-300/400 in Step 7 Classic V5.5 SP3)
     Registrierung notwendig  Project (STEP 7 V5.5 SP3) (18,2 MB)
      Documentation (11,9 MB)

Further Information
Universal Diagnostic Block and HMI Template for AS-Interface Safety Monitor
Convenient Command Interface for CP343-2 (P) and DP/ AS-i (F) Links for AS-Interface

Last Changes
Project for S7-300 in TIA Portal V13 SP1 added.


Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.