×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 51612728, Entry date: 08/03/2011
(1)
Rate

SIMATIC PDM V6.1 Released for Delivery

  • Entry
  • Associated product(s)

Version 6.1 of the SIMATIC PDM Process Device Manager is now released for delivery. The special features of SIMATIC PDM V6.1 are: numerous new and improved functions, updated device descriptions, plus integration of additional field devices.

1 Product description

1.1 Classification/Application area

SIMATIC PDM is by now firmly established on the market as a universal, non-proprietary tool for configuring, parameterizing, commissioning, diagnosing and maintaining intelligent field devices (sensors and actuators) and field components (remote I/Os, multiplexers, control room devices, compact controllers). With more than 2000 device descriptions for a range of devices from more than 200 manufacturers worldwide, SIMATIC PDM has one of the largest library of all parameterization tools available on the market. Version 6.1 further expands the number of supported devices and also extends, rounds off and improves the functionality, performance and ease of operation of SIMATIC PDM.

In the context of SIMATIC PCS 7 you can also use SIMATIC PDM V7.0 instead of SIMATIC PDM V6.1. However, for projects without "FOUNDATION Fieldbus" communication we recommend the use of SIMATIC PDM V6.1.

1.2 Product features

Performance, Ease of Operation and Functions

  • The operator interface and the control functions are comparable with SIMATIC PDM V6.0 + SP5
  • Enabling of the print function in SIMATIC PDM Single Point now permits printing out the parameter overview with this product variant as well
  • In addition to the HART revisions 5 and 6, all relevant commands and functions of HART revision 7 are now supported
  • Diagnosis and parameterization of HART field devices with Wireless-HART communication by integration of the HART OPC server V3.2 and support of the HART revision 7
  • Acceleartion of the HART communication by means of SHC-Mode, based on the "HART on PROFIBUS" specification of the PROFIBUS & PROFINET International organization.
    • SHC-Mode depends on the hardware used
    • SIMATIC PDM detects if the SHC-Mode can be used
    • 8-channel HART modules of ET 200M and HART modules of ET 200iSP support the SHC-Mode as from firmware version 3 onward
  • Function "HART-Long-TAG" for HART devices according to Revision < 6
    • TAG Names with up to 32 characters can be created via the parameter "Message" of the field devices
    • Use of the 32-character TAG name in the process device network view and the process device plant view
  • Updating and adding of device descriptions of already integrated field devices and components
  • Integration of additional field devices and libraries:
    • EDD Library of PROFIBUS & PROFINET International
    • Device library of the HART Communication Foundation (HCF)
    • Additional devices of well-known suppliers
  • Device replacement with devices that correspond to the PA-Profile 3.0.2
    • Active support of devices developed acc. to the "Profile for Process Control Devices Version 3.02" specification
    • Devices to PA-Profile 3.0.2 can replace older devices corresponding to the manufacturer's specifications without having to change the configuration, as a result of the compatibility mode for cyclical communication (PROFIBUS ID adaptation)
    • Significant reduction of the communication times with devices due to block transmission (View Objects) of parameters with writing/reading
  • EDD Exchange during device maintenance
    • EDDs of the devices in the projects are exchangeable
    • Support of version jumps of devices as well as the exchange of non-compatible device descriptions
  • "Ethernet" communication
    • Siemens series 7 analytic devices with "Ethernet" communication can be processed
    • Using a SIMATIC PDM stand-alone service tool on a mobile computer on Industrial Ethernet you can process several PROFIBUS networks connected to Industrial Ethernet via IE/PB LINK PN IO gateways
  • Licenses are supplied on a USB stick

1.3 Product packages

SIMATIC PDM Single Point V6.1

SIMATIC PDM Single Point V6.1 supports the following types of communication:

  • PROFIBUS DP/PA
  • HART Communication (modem, RS 232)
  • Modbus

The functionality of this minimum configuration is matched to processing a single field devices via point-to-point coupling. All functions of this device are supported as defined in the device description. These functions include:

  • Unrestricted device selection/administration of the device library
  • Parameterization and diagnosis as defined in the device description
  • Export and import of parameter data
  • Device identification
  • Lifelist
  • Print function for parameter list

The following system functions of SIMATIC PDM Basic V6.1 are not available with SIMATIC PDM Single Point V6.1:

  • EDD-based diagnosis in the Lifelist
  • Project processing
  • Memory function (only export and import of parameter data)
  • Logging function
  • Communication with HART field devices via remote I/Os

SIMATIC PDM Single Point V6.1 cannot be expanded, neither via TAG option or PowerPack, nor functionally (e.g. on SIMATIC PDM Basic V6.1 or with routing via S7-400). Upgrading to another product variant is also not possible.

SIMATIC PDM Basic V6.1

If the system requirements are met, SIMATIC PDM Basic V6.1 can be used for the stand-alone operation on any comuter (PC/Notebook) with a local connection to bus segments, or with a direct connection to the device. The product package includes all the functions required for the control and parameterization of the devices. It is released for the following types of communication:

  • PROFIBUS DP/PA
  • HART Communication (modem, RS 232 and via PROFIBUS)
  • Modbus
  • SIREC-Bus
  • SIPART DR
  • Ethernet

SIMATIC PDM Basic V6.1 is a basic module for individual configuration and can be expanded with all optional product components, TAG options and PowerPacks for SIMATIC PDM V6.1. Without TAG expansion SIMATIC PDM Basic V6.1 can administrate projects with up to 4 TAGs.

The use of the following functions requires at least 128 TAGs:

  • Modification logbook
  • Calibration log
  • Detailed diagnosis in the Lifelist

SIMATIC PDM Service V6.1

This product package is configured for mobile use in service and maintenance for projects with up to 128 TAGs. It offers the service technician all communication types and functions of SIMATIC PDM Basic V6.1, plus special service functions such as modification logbook, calibration log or detailed diagnosis in the Lifelist

SIMATIC PDM Service V6.1 can be expanded with the functional options "Integration in STEP 7/PCS 7", "Routing via S7-400" and "Communication via Standard-HART-Multiplexer" (see under Optional Product Components), as well as with SIMATIC PDM PowerPacks.

SIMATIC PDM S7 V6.1

SIMATIC PDM S7 V6.1 is a product package for projects with up to 128 TAGs and matched for use of SIMATIC PDM in a SIMATIC S7 configuration environment. In addition to SIMATIC PDM Service V6.1, it also features the functionality for integration in the Hardware Configurator (HW Config) of STEP 7 (corresponds to the option "Integration in STEP 7/PCS 7").

SIMATIC PDM S7 V6.1 can be expanded with the functional options "Routing via S7-400" and "Communication via Standard-HART-Multiplexer" (see under Optional Product Components), as well as with SIMATIC PDM PowerPacks.

SIMATIC PDM PCS 7 V6.1

The SIMATIC PDM PCS 7 V6.1 product package is designed for projects with up to 128 TAGs. It expands the functionality of SIMATIC PDM Service V6.1 with routing from the central engineering system to the devices in the field and integrates SIMATIC PDM by means of HW Config into the SIMATIC PCS 7 configuration environment.

SIMATIC PDM PCS 7 V6.1 can be expanded with the option "Communication via Standard-HART-Multiplexer" (see under Optional Product Components) and SIMATIC PDM PowerPacks.

1.4 Optional Product Components

SIMATIC PDM Option Integration in STEP 7/PCS 7

This option serves to integrate SIMATIC PDM into a SIMATIC S7 or SIMATIC PCS 7 configuration environment. It enables SIMATIC PDM to be started directly from the Hardware Configurator (HW Config) in STEP 7/SIMATIC PCS 7.

SIMATIC PDM Option Routing via S7-400

For overall plant configuration, parameterization, commissioning and diagnosis of the field devices you also require the option "SIMATIC PDM Routing via S7-400", in addition to the option "SIMATIC PDM Integration in STEP 7/PCS 7". It enables processing each field device that can be parametrized with EDD via the various bus systems and remote I/Os, from a central engineering system.

SIMATIC PDM Option Communication via Standard HART Multiplexer

This option enables SIMATIC PDM to use the HART-OPC Server for the communication with HART field devices via HART Multiplexer.

1.5 TAG Options / PowerPacks

One TAG corresponds to one SIMATIC PDM object, representing individual field devices or field components within one project, e.g. measuring devices, positioners, switching devices or remote I/Os. TAGs are also of relevance for the diagnosis with the Lifelist of SIMATIC PDM. All identified devices capable of diagnosis, whose detailed diagnosis has ben implemented via the device description (EDD), are counted as TAGs in this case.

PowerPacks enable the SIMATIC PDM product range (except SIMATIC PDM Single Point V6.1) to be equipped with additional TAGs. PowerPacks are available for the TAG expansion to 512, 1 024, 2 048 and unlimited TAGs.

In contrast to PowerPacks, the TAG options are only suitable for individual SIMATIC PDM product configurations, starting from the SIMATIC PDM Basic V6.1 basic module. The SIMATIC PDM TAG options enable SIMATIC PDM Basic V6.1 to be expanded from 4 TAGs to 128, 512, 1 024 or 2 048 TAGs, and, with the aid of an additive PowerPack for SIMATIC PDM V6.1, to unlimited TAGs.

1.6 Demo software

SIMATIC PDM V6.1 is also available in a demo version for demonstration purposes. Online communication and memory functions are not available with this product.

1.7 Compatibility

1.7.1 Software compatibility

 SIMATIC PDM V6.1 is compatible with the following Windows operating systems:

  • Windows XP Professional SP3 (Ge/En/multilingual)
  • Windows Server 2003 (Standard Edition) R2 SP2 (Ge/En/multilingual)

The table below supplements the information in the readme file concerning compatibility (executability and/or the project data) between SIMATIC PDM V6.1 and different versions of SIMATIC STEP 7 and SIMATIC PCS 7:
 

Product Version STEP 7 V4.x PCS 7 V5.x STEP 7 V5.x PCS 7 V6.x PCS 7 V7.x
SIMATIC PDM V6.1 no no V5.3+SP2
V5.4+SP5
V5.5
V5.5+SP1
V6.1+SP4 V7.1
V7.1+SP1
V7.1+SP2
V7.1+SP3
V7.1+SP4

1.7.2 Compatibility of the device descriptions

In principle, the device descriptions previously used with SIMATIC PDM V6.0 + SP5 will also work with SIMATIC PDM V6.1. However, adaptations in the international standards and specifications have lead to changes in the basic libraries of SIMATIC PDM. The Device Library 1#2011 included with SIMATIC PDM V6.1 integrates the following updated or corrected libraries of international organizations:

  • EDD Library V2.0 of PROFIBUS & PROFINET International
  • Device Library 04/2010 of the HART Communication Foundation (HCF)

Due to the fact that many device descriptions make use of these libraries, it is necessary to at least newly import the device descriptions of the field devices used in the projects. As a result of the adaptations, error messages can appear in isolated cases with the interpretation of device descriptions in which non-changeable texts are included. In these cases please contact the relevant device manufacturer to obtain an update of the device description concerned. We will publish separate bulletins on the topic of changes/updates of the Device Library 1#2011.

1.7.3 Hardware compatibility

The compatibility of SIMATIC PDM V6.1 with communication processors (CPs) for PROFIBUS, Industrial Ethernet and HART communication has not been checked explicitly. The product-specific releases for CPs will be published in conjunction with the releases for SIMATIC PDM V6.1 for the different versions of SIMATIC PCS 7.

It follows that for stand-alone operation or for use in a central SIMATIC PCS 7 Engineering Station the following communication modules are also released for SIMATIC PDM V6.1:
 

Industrial Ethernet Windows Server 2003 Windows XP Remarks
CP 1613 A2 yes yes order no. 6GK1 161-3AA01
CP 1623 yes yes order no. 6GK1 162-3AA00
IE/PB LINK PN IO gateway yes yes order no. 6GK1 411-5AB00
Realtek RTL8111CP Ethernet Controller 10/100/1000 Mbit/s yes yes Onboard interface in SIMATIC PCS 7 Workstation type IPC547C
Intel network card 10/100/1000 Mbit/s with PCI port yes yes order no.. A5E00718412
Intel network card 10/100/1000 Mbit/s with PCIe port yes yes order no. A5E01579552

The following PROFIBUS communication modules are released for the local data access of SIMATIC PDM V6.1 on PROFIBUS:
 

PROFIBUS Windows Server 2003 Windows XP Remarks
CP 5611 yes yes order no. 6GK1 561-1AA00
CP 5611 A2 yes yes order no. 6GK1 561-1AA01
CP 5711 yes yes order no. 6GK1 571-1AA00
CP 5613 A2 yes yes order no. 6GK1 561-3AA01
PC Adapter USB yes yes order no. 6ES7 972-0CB20-0XA0 in combination with a separate plug-in power supply, order no. 6ES7972-0CA00-0XA0
order no. 6GK1571-1AM00 (no separate plug-in power supply)

1.7.4 Communication modules from other manufacturers

It is not explicity forbidden to use Siemens communication modules that are not listed in the above tables, or communication modules from other manufacturers. However, the use of SIMATIC PDM V6.1 in combination with modules that have not explicitly been released is at your own risk. Siemens accepts no liability for defects or damages that might arise as a result of their use. Delivery and support of non-Siemens components are not handled by Siemens, but only through the respective manufacturer or their distributors.

2 Ordering information

2.1 Ordering data for SIMATIC PDM V6.1
 

Product Name Order No.
Product packages
SIMATIC PDM  Single Point V6.1
For control and parameterization of one field device, communication via PROFIBUS DP/PA, HART Modem or Modbus; incl. 1 TAG, multilingual (Ge, En, Fr, It, Sp, Zh), software class A, executes under Windows XP Professional/Server 2003, cannot be expanded in function or TAG option/PowerPack, Floating License for 1 User
6ES7658-3HX16-0YA5
SIMATIC PDM  Basic V6.1
For control and parameterization of field devices and components, communication via PROFIBUS DP/PA, HART (modem, RS 232, PROFIBUS), SIREC bus, SIPART-DR, Modbus or Ethernet; incl. 4 TAGs, multilingual (Ge, En, Fr, It, Sp, Zh), software class A, executes under Windows XP Professional/Server 2003, functional and TAG option/PowerPack expansion, Floating License for 1 User
6ES7658-3AX16-0YA5
SIMATIC PDM  Service V6.1
for stand-alone applications in service and maintenance, with
• SIMATIC PDM Basic
• 128 TAGs,
multilingual (Ge, En, Fr, It, Sp, Zh), software class A, executes under Windows XP Professional/Server 2003, functional and TAG option/PowerPack expansion, Floating License for 1 User
6ES7658-3JX16-0YA5
SIMATIC PDM  S7 V6.1
for use in a SIMATIC S7 configuration environment, with
• SIMATIC PDM Basic
• Integration in STEP 7/PCS 7
• 128 TAGs
multilingual (Ge, En, Fr, It, Sp, Zh), software class A, executes under Windows XP Professional/Server 2003, functional and TAG option/PowerPack expansion, Floating License for 1 User
6ES7658-3KX16-0YA5
SIMATIC PDM  PCS 7 V6.1
for integration into the Engineering Toolset of the SIMATIC PCS 7 Engineering System, with
• SIMATIC PDM Basic
• Integration in STEP 7/PCS 7
• Routing via S7-400
• 128 TAGs
multilingual (Ge, En, Fr, It, Sp, Zh), software class A, executes under Windows XP Professional/Server 2003, functional and TAG option/PowerPack expansion, Floating License for 1 User
6ES7658-3LX16-0YA5
Optional Product Components
Integration in STEP 7/PCS 7 V6.1
required only for the integration of SIMATIC PDM in HW Config,
multilingual (Ge, En, Fr, It, Sp, Zh), software class A, executes under Windows XP Professional/Server 2003, Floating License for 1 User
6ES7658-3BX16-2YB5
Routing via S7-400 V6.1
multilingual (Ge, En, Fr, It, Sp, Zh), software class A, executes under Windows XP Professional/Server 2003, Floating License for 1 User
6ES7658-3CX16-2YB5
Communication via Standard HART Multiplexer V6.1
multilingual (Ge, En, Fr, It, Sp, Zh), software class A, executes under Windows XP Professional/Server 2003, Floating License for 1 User
6ES7658-3EX16-2YB5
TAG Options / PowerPacks
SIMATIC PDM TAG Option V6.1
for TAG expansion, in addition to SIMATIC PDM Basic V6.1
software class A, executes under Windows XP Professional/Server 2003, Floating License for 1 User
 
• up to 128 TAGs 6ES7658-3XA16-2YB5
• up to 512 TAGs 6ES7658-3XB16-2YB5
• up to 1 024 TAGs 6ES7658-3XC16-2YB5
• up to 2 048 TAGs 6ES7658-3XD16-2YB5
SIMATIC PDM PowerPack V6.1
for TAG expansion; for any product packages of SIMATIC PDM V6.1, except SIMATIC PDM SinglePoint
software class A, executes under Windows XP Professional/Server 2003, Floating License for 1 User
 
• from 128 TAGs to 512 TAGs 6ES7658-3XB16-2YD5
• from 512 TAGs to 1024 TAGs 6ES7658-3XC16-2YD5
• from 1024 TAGs to 2048 TAGs 6ES7658-3XD16-2YD5
• from 2048 TAGs to TAGs unlimited 6ES7658-3XH16-2YD5
Demo software
SIMATIC PDM Demo V6.1
without online communication and memory functionality
multilingual (Ge, En, Fr, It, Sp, Zh), software class A, executes under Windows XP Professional/Server 2003
6ES7658-3GX16-0YC8

2.2 Upgrade Package/Software Update Service

The SIMATIC PDM Upgrade V6.0 to V6.1 enables you to upgrade all product variants and combinations of SIMATIC PDM V6.0 to V6.1. Alternatively you can also purchase a SIMATIC PDM Software Update Service (SUS) for upgrading.
 

Product Name Order No.
SIMATIC PDM Upgrade/Software Update Service
SIMATIC PDM  Upgrade V6.0 to V6.1
for all product variants and combinations, multilingual (Ge, En, Fr, It, Sp, Zh), software class A, executes under Windows XP Professional/Server 2003,, Floating License for 1 User
6ES7651-5CX16-0YE5
SIMATIC PDM  Software Update Service
Subscription for one year with automatic extension; the precondition is the latest software version
6ES7658-3XX00-0YL8

3 Information and documentation

Catalog

Information and ordering data for SIMATIC PDM V6.1 are expected to be available by Oct. 2011 in the Industry Mall (under ES Software in the branch SIMATIC PCS 7, System Components, Engineering System).

Internet

For more information on SIMATIC PDM as well as the device descriptions for later installation please see the Internet at:

http://www.siemens.com/simaticpdm

Product documentation / Manual

The product documentation is supplied in electronic form together with the SIMATIC PDM software.

Important preliminary information is available from the following readmes:

pdmbase-readme.wri ( 56 KB )

pdmdevices-readme.wri ( 7 KB )

4 Supplementary product-specific conditions for permission to use software

In addition to the "General terms and conditions for permission to use software for automation and drives" please note the special product-specific terms and conditions for SIMATIC PDM:

Warranty and liability

Siemens will not provide warranty for the following Device Descriptions (DDs) and for the correct interaction of these DDs with the associated devices. Siemens is explicitly not liable for damages that arise from the use of the following DDs in conjunction with the associated devices:

  • Device-specific DDs for non-Siemens devices (Siemens warranty only up to interface)
  • Non device-specific DDs, e.g. DDs that correspond to the PROFIBUS PA profiles, resp. the Universal or Common Practice Commands of HART.
  • DDs of the HCF library on the DVD with the Device Library (DVD 2/2)
  • DDs which have been integrated via catalog import.

Important note concerning the device descriptions supplied with SIMATIC PDM

The EDD Device Library supplied with SIMATIC PDM contains device descriptions (EDDs) from Siemens and other device manufacturers. However, Siemens is only responsible for device descriptions of the Siemens devices. The device descriptions of other manufacturers are supplied by Siemens free of charge for convenience of handling. For the included device descriptions of other manufacturers Siemens only guarantees correct copies on the data carrier supplied.

The licensee is authorized to use the DDs of these devices in accordance with the "General Conditions for the Licensing of Software for Automation and Drives" like a Trial License. The licensee can exercise this right of use as long as he has the right of use for the SIMATIC PDM software.

5 Customer Support  

Siemens can provide Service & Support for any phase of a project: from planing and commissioning right up to maintenance and modernization. An overview of our services is available on the Internet at:

http://www.siemens.de/automation/csi_de_WW/service (national)
http://www.siemens.com/automation/csi_en_WW/service (international)

Support for SIMATIC PDM V6.1 is available from our Technical Support (Hotline) of Automation and Drives via the support request procedure:

http://www.siemens.de/automation/csi_de_WW/support_request (national)
http://www.siemens.com/automation/csi_en_WW/support_request (international)
 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.
Support to the statistics
With this function the IDs found are listed according to number (format .txt).

Generate list
Copy URL
Display page in new design
mySupport Cockpit