×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 51696778, Entry date: 08/02/2011
(8)
Rate

Service Packs 1 for STEP 7 V11

  • Entry
  • Associated product(s)

DESCRIPTION:

The Service Packs are applicable to the following products:

  • STEP 7 Professional V11
  • STEP 7 Basic V11

New features and changes compared to earlier versions are described in the delivery release for STEP 7 V11 SP1 (entry ID 51774795)

Installation instructions

  • If your installation comprises several products based on the TIA Portal (e.g. STEP 7 V11 and WinCC V11), all the products must be upgraded to Service Pack 1 (see entry ID 51706933)
  • Service Pack 1 of WinCC Basic V11 is part of STEP 7 Professional/Basic V11 SP1.
  • We recommend to install the latest update after installing the Service Pack 1 (see entry ID 52258326)

STEP 7 Professional V11:
Free download of Service Pack 1 for STEP 7 Professional V11:

SIMATIC_STEP_7_Professional_V11.001  ( 665600 KB )  

SIMATIC_STEP_7_Professional_V11.002  ( 665600 KB )

SIMATIC_STEP_7_Professional_V11.003  ( 665600 KB )

SIMATIC_STEP_7_Professional_V11.004  ( 665600 KB )  

SIMATIC_STEP_7_Professional_V11.005  ( 289279 KB )

  SIMATIC_STEP_7_Professional_V11.exe  ( 1811 KB )  

This free download contains the Service Pack 1 for STEP 7 Professional V11 and can only be installed, if STEP 7 Professional V11 is installed already.
The download comprises several files. Please download all the files first and then execute the file ending with .exe. After that the parts will be joined together and you can execute the Setup.

 

STEP 7 Basic V11:
Free download of Service Pack 1 for STEP 7 Basic V11:

SIMATIC_STEP_7_Basic_V11.001  ( 665600 KB )

SIMATIC_STEP_7_Basic_V11.002  ( 665600 KB )

SIMATIC_STEP_7_Basic_V11.003  ( 665600 KB )

SIMATIC_STEP_7_Basic_V11.004  ( 665600 KB )

SIMATIC_STEP_7_Basic_V11.005  ( 233711 KB )  

SIMATIC_STEP_7_Basic_V11.exe  ( 1811 KB )

This free download contains the Service Pack 1 for STEP 7 Basic V11 and can only be installed, if STEP 7 Basic V11 is installed already.
The download comprises several files. Please download all the files first and then execute the file ending with .exe. After that the parts will be joined together and you can execute the Setup.

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
http://www.siemens.com/industrialsecurity.