×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 51772626, Entry date: 08/02/2011
(0)
Rate

Hotfix 12 (Update) for WinCC V6.2 SP3 and WinCC V6.2 SP3 ASIA

  • Entry
  • Associated product(s)

DESCRIPTION:
Download of Hotfix 12 for SIMATIC WinCC V6.2 SP3 and SIMATIC WinCC V6.2 SP3 ASIA

Installation Prerequisite:

  • SIMATIC WinCC V6.2 Service Pack 3
  • SIMATIC WinCC V6.2 Service Pack 3 ASIA

Check first what WinCC components are installed on the computer. This information can be found in the Windows "Control Panel" under "Add or Remove Programs". Then, depending on the WinCC components installed, download the required Hotfix.

Information about Hotfix 12:

Please observe the installation and usage instructions in the following PDF file:

WinCC_V62_SP3_HF12_Readme.pdf ( 234 KB )
 

Download of the Hotfix:
The Hotfix is provided as a self-extracting ZIP archive. Download the file into a folder on your PC and start the extraction by double-clicking on the file. Then select the target folder and click on the "Extract" button.    

Please be aware of the file size.  

 

 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.