Entry type: FAQ, Entry ID: 51930734, Entry date: 08/31/2011

What must be considered when using the SIMATIC S7 FM354 module with incremental encoder?

  • Entry
  • Associated product(s)
When using an incremental encoder the resolution of the encoder must not exceed 8000 steps/rotation. If the resolution is exceeded (10,000 steps/rotation, for example), then the zero mark monitoring function can no longer be executed correctly.