×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ, Entry ID: 51944745, Entry date: 11/24/2011
(0)
Rate

How do you link the AS-i Slaves to an S7-300 CPU with integrated PROFINET interface using the IE/AS-i Link?

  • Entry
  • Associated product(s)

Description
This entry provides sample programs and documentation for linking IE/AS-i slaves to an S7-300 CPU with integrated PROFINET interface using an IE/AS-i Link.

The sample program consists of a STEP 7 project that contains the configuration of the SIMATIC S7 station and the IE/AS-i Link.

IE_AS-i_Link.zip ( 624 KB )

The document below contains the following:

  • An overview of the sample program and plant configuration used to create the sample program.
  • Information about installing and commissioning the sample program.
  • Information about how to use the sample programs.
  • Other notes, tips and tricks, etc.

DP_configuration_IE_AS-i_Link_en.pdf ( 344 KB )

Further Information
More information about linking AS-i slaves to a SIMATIC S7 using the IE/AS-i Link is available in the Entry IDs below:
 

Description Entry ID
CPU-CPU Communication with SIMATIC Controllers (Compendium) 20982954
SIMATIC NET gateway IE/PB Link 7851748
Manual SIMATIC NET IE/AS-INTERFACE LINK PN IO 22712154
SIMATIC S7-300 CPU 31xC and CPU 31x: Technical data 12996906
Automation System SIMATIC S7-400 CPU Specifications 53385241

Security information
In order to protect plants, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art industrial security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about industrial security, please visit
http://www.siemens.com/industrialsecurity.