×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 51945518, Entry date: 08/12/2011
(0)
Rate

Safety Rated Sequential Start-ups, using SIMATIC Safety Matrix

  • Entry
  • Associated product(s)

Objective of the Application
Although most facilities embrace ANSI/ISA 84.00.01-2004 (IEC 61511) and the Safety Life Cycle (SLC) as the best way to comply with regulatory requirements (Like OSHA in the USA for example), there are specific instances when most operations deviate from the standards i.e. during start-ups, shut-downs and process transitions. Bypassing, inhibiting or masking is a common practice during these plant conditions, seriously compromising the Safety Integrity of the substituted functions.

The presented project example examines how Simatic Safety Matrix could be used to simplify the development and implementation of automated permissive sequences without the need to remove Safety Instrumented System (SIS) protections, or compromise the Safety Integrity Level (SIL) of any Safety Instrumented Function (SIF), whilst still including verification and validation as required by safety standards.

Main Contents of this Application Note
The following issues are discussed in this application note:

  • The timing and process variable constraints of an override (Changing variable thresholds or limits)
  • Priority in intersections classes/conditions
  • Causes, type of timers and effect monitoring

Validity
 
This document is valid for PCS 7 version V7.1 SP1 or higher and Safety Matrix V6.2

Downloads

Content of the Downloads

Download

Safety Rated Sequential Start-ups, using SIMATIC Safety Matrix 51945518_Application_PCS7_Sequential_Start-up_en.pdf ( 1931 KB )

History

Output

Modifications

08/ 2011

First release

 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.
Support to the statistics
With this function the IDs found are listed according to number (format .txt).

Generate list
Copy URL
Display page in new design
mySupport Cockpit